Public lighting renewal in Roztoky
Safe and sustainable cities thanks to Philips SunStay

Public lighting renewal in Roztoky

Solar powered street lighting

The city of Roztoky modernized its public lighting with Signify LED technology

Smart LED lighting with Interact remote management in Roztoky has provided safer streets, lower costs, and a more environmentally friendly approach.  

Illuminazione stradale efficiente e sostenibile

"The project delivered 74% energy savings, annual savings of CZK 200,000, and improved safety. In addition, thanks to the Interact City system, we have control over when and where lighting is needed. "

- Ing. Ivan Goll, Secretary of the City of Roztoky

customer challenge

Customer Challenge

The original public lighting in Roztoky was outdated, had high energy consumption, and produced excessive light pollution, increasing costs and negatively affecting the environment and residents’ well-being. 

 

The city was looking for a solution aligned with modern standards and environmental criteria, respecting the appearance of public space while enabling future integration of smart systems. 

 

The project had to be implemented quickly without significant disruption, ensuring precise planning, cost calculation, and flexible coordination with suppliers. 

Solution

For the modernization, Philips DigiStreet, CitySoul, ClassicStreet, and Villa LED luminaires were used, predominantly DigiStreet (BGP76x) with optical efficiency up to 90%, directing light downward and equipped with shields to reduce light spill.  


Warm white light was used: 2200 K for parks and quiet zones, 2700 K for main routes and side streets, reducing light pollution and ensuring comfortable color perception. The Interact City system enabled remote control, dimming, predictive maintenance, and rapid response to faults.    

"The city can now flexibly respond to rising energy prices, for example by introducing dimming regimes or adjusting switching times. Lighting is operated only when and where it is actually needed."


Ing. Ivan Goll, Secretary of the City of Roztoky

Energy savings

Reduction of total lighting system power consumption by 41% thanks to the switch from discharge lamps to OptiVision LED technology.

Annual cost savings

Approximately EUR 8.000 saved on energy annually (at 0,089 EUR/kWh and 4.100 hours/year).

Reduced light disturbance to surroundings

Asymmetric optics with integrated shields and light spill control helped reduce unwanted light outside the sports facility.

Efficient operation

Lighting is used only when and where needed. Ability to adjust light levels based on activity type improved operational efficiency.

Smart control

The Dynalite control system enabled easy operation, preset lighting scenes, and dimming and instant restart in case of a power outage.

Ready for the future

The modern LED infrastructure with intelligent controls is scalable and ready to meet future technological requirements of the sport facility

Discover other case studies

The KNVB Campus - Zeist, The Netherlands

Interact and Certified System Integrator Oostendorp Nederland B.V. teamed up to transform the KNVB Campus in Zeist – the beating heart of Dutch football.

Optimizing a Hoog Op Tennis Club’s lighting

Signify Certified System Integrator, Oostendorp Nederland, delivered an innovative, connected lighting solution to enhance the member experience at Hoog Op Tennis Club.

Grand Stade de Tanger by Lamalif

The Ibn Batouta Stadium in tangier stands as a true showcase of Signify’s cutting-edge lighting technology. Featuring Arenavision with BVP428 luminaires for the pitch and ClearFlood BVP650 for the stands, and Unistrip BCP383 for the façade. The stadium delivers unmatched visibility, safety, and ambiance for players and fans alike. This state-of-the-art system positions the venue at the forefront of global sports infrastructure, ready to shine brilliantly for AFCON 2025, the 2030 World Cup, and millions of passionate fans across the continent.

Ekinox Arena

Philips ArenaVision LED sports lighting in Ekinox Arena

Lacrosové hřiště Radotín

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Smart office lighting – Arrival

Bus operator Arriva achieved complete control over their lighting and reduced energy usage thanks to Interact Pro.

Sevens Stadium - UAE

Lighting the future of sport with sustainability in every kick

A focus on fan experience and new revenue streams – Optus Stadium

With the goal of creating the ultimate fan experience, the recent all-LED lighting and Interact Sports software at Optus Stadium makes it the premier multipurpose venue in the Southern Hemisphere.

Smart lighting for best multipurpose arena experience – Buesa Arena

The Fernando Buesa Arena in Spain converted 100% of the lighting to LED and connected via a standard wired connection, all remotely controlled and managed with Interact Sports.

Fan experience and easy control – Allianz Stadium

Interact Sports offers an easy-to-use dashboard to control all the lighting systems in Allianz Stadium. Allianz now enjoys increased fan engagement, high-quality broadcast capabilities and new revenue potential.

Melbourne Cricket Ground by Lightmoves

The Melbourne Cricket Ground (MCG), a 100,000 person stadium in Melbourne, hosts major international, national, and local sporting events and concerts, including the Boxing Day Test, AFL Grand Final, and performances by artists such as AC/DC and Taylor Swift. The project involved retrofitting 12 electrical zones across 7 levels, replacing the legacy control system with a Dynalite solution to deliver enhanced, venue-wide control.

Connected stadium – fan experience

As Turkey’s largest multipurpose venue, the Sinan Erdem Arena has installed Interact Sports management software to bring a connected stadium concept to life using connected LED lighting infrastructure.

Starting a project?

Starting a project?

We’d love to hear from you.