Global - English
A World Première in Ekinox Arena
A World Première in Ekinox Arena

A World Première in Ekinox Arena

Lighting the Ekinox indoor arena

ArenaVision LED creates special entertainment lighting effects that would normally require dedicated stage-lighting fixtures

teaser

“We needed a lighting solution for both basketball games andshows. Hence, ArenaVision LED floodlights had to illuminatenot only the playing area but also the stage and public area.”

- Fabrice Pacquelet, director of JL Bourg basketball club director

teaser

Customer challenge

In 2011, Bourg-en-Bresse Agglomeration (BBA) decided to renovate its exhibition center Ainterexpo. The center was built in the 1970s and had three halls. Beginning of this year a fourth hall was added with a space of 9,940 m2. Thanks to the modularity of its stands and its technical platform, the main hall can accommodate performances in 360°. Only an exceptional lighting system could match this modernity – that is how ArenaVision LED became involved.

The right lighting

 

The floodlights not only had to illuminate the playing area but also the stage area and the public space. It was also important for the JL Bourg basketball club to be able to switch the floodlights off completely and then switch it on again a few seconds later for the show element prior to the game, which had not been possible with metal halide lamps. ArenaVision LED can get to full power in just a few seconds.

Benefits

Benefits
ArenaVision LED

ArenaVision LED

Philips ArenaVision LED floodlighting system is an innovative LED pitch-lighting solution supporting the latest TV broadcasting standards and featuring a control platform to create...

Photo gr

Lighting the Ekinox indoor arena

The team

Client

Bourg-en-Bresse Agglomeration

Architect

Pierre Barillot

Installer

INEO

Photographer

Grégory Picout

Discover other case studies

The KNVB Campus - Zeist, The Netherlands

Interact and Certified System Integrator Oostendorp Nederland B.V. teamed up to transform the KNVB Campus in Zeist – the beating heart of Dutch football.

Optimizing a Hoog Op Tennis Club’s lighting

Signify Certified System Integrator, Oostendorp Nederland, delivered an innovative, connected lighting solution to enhance the member experience at Hoog Op Tennis Club.

Grand Stade de Tanger by Lamalif

The Ibn Batouta Stadium in tangier stands as a true showcase of Signify’s cutting-edge lighting technology. Featuring Arenavision with BVP428 luminaires for the pitch and ClearFlood BVP650 for the stands, and Unistrip BCP383 for the façade. The stadium delivers unmatched visibility, safety, and ambiance for players and fans alike. This state-of-the-art system positions the venue at the forefront of global sports infrastructure, ready to shine brilliantly for AFCON 2025, the 2030 World Cup, and millions of passionate fans across the continent.

Lacrosové hřiště Radotín

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Smart office lighting – Arrival

Bus operator Arriva achieved complete control over their lighting and reduced energy usage thanks to Interact Pro.

Sevens Stadium - UAE

Lighting the future of sport with sustainability in every kick

A focus on fan experience and new revenue streams – Optus Stadium

With the goal of creating the ultimate fan experience, the recent all-LED lighting and Interact Sports software at Optus Stadium makes it the premier multipurpose venue in the Southern Hemisphere.

Smart lighting for best multipurpose arena experience – Buesa Arena

The Fernando Buesa Arena in Spain converted 100% of the lighting to LED and connected via a standard wired connection, all remotely controlled and managed with Interact Sports.

Fan experience and easy control – Allianz Stadium

Interact Sports offers an easy-to-use dashboard to control all the lighting systems in Allianz Stadium. Allianz now enjoys increased fan engagement, high-quality broadcast capabilities and new revenue potential.

Melbourne Cricket Ground by Lightmoves

The Melbourne Cricket Ground (MCG), a 100,000 person stadium in Melbourne, hosts major international, national, and local sporting events and concerts, including the Boxing Day Test, AFL Grand Final, and performances by artists such as AC/DC and Taylor Swift. The project involved retrofitting 12 electrical zones across 7 levels, replacing the legacy control system with a Dynalite solution to deliver enhanced, venue-wide control.

Connected stadium – fan experience

As Turkey’s largest multipurpose venue, the Sinan Erdem Arena has installed Interact Sports management software to bring a connected stadium concept to life using connected LED lighting infrastructure.

Starting a project?

Starting a project?

We’d love to hear from you.