New opportunities with smart pitch lighting
New opportunities with smart pitch lighting

New opportunities with smart pitch lighting

Portugalete football club

Bilbao, Spain

The Portugalete football team, a 3rd league team with an average spectator draw of 4000 people per home match, was interested in installing a flexible lighting system that would help the team attract additional visitors and open up new revenue streams. In addition, the team needed to be able to play at night while adhering to TV broadcasting requirements and league rules for illumination.

“Vision is perfect, without shadows. The playing conditions are really good and we can see from the field that there are more fans in the stands. And with our new lighting, we can now host national matches.”

- Jon Moya, Captain of Club Portugalete

Customer challenge

In Campo de La Florida, the soccer field in Portugalete, a suburb of Bilbao in Spain, the football pitch owners realized they had a serious problem when the team qualified for the Copa del Rey football tournament and a Third Division team was scheduled to play them at home. Until then, the team had always played their matches during the day and had no need for nighttime illumination. But Federation rules required the teams to play at night and in front of television cameras, making it necessary to install a flexible lighting system that could be easily managed and controlled, and is also compliant with broadcasting standards.

Data-driven decisions for improved performance

 

Interact Sports lighting management software, configured specifically to manage lighting at recreational sports training facilities, proved to be the right solution for the club.

 

With the option of choosing among different programmable scenes, the lighting management application allows for remote configuration of the lighting and the ability to pre-set light levels for the entire facility. With three distinct light settings, La Florida can adjust lighting levels for match days and training, as well as setting a low light level for cleaning and maintenance purposes. These settings, along with the possibility to light only half of the pitch, contribute to energy savings of 33% for the club compared to the previous lighting system.

 

Connected LED lighting enables the collection of data, allowing the club to analyze lighting performance and usage, and subsequently make data-driven decisions to improve operations. Outage information can be seen on the Interact Sports dashboard for quick response time and reduced downtime.

 

The Portugalete football club can now host national matches and is growing their spectator numbers thanks to the new lighting. Furthermore, they’ve reduced energy costs with the installation of LED lighting combined with simple and intuitive lighting controls.

Discover other case studies

The KNVB Campus - Zeist, The Netherlands

Interact and Certified System Integrator Oostendorp Nederland B.V. teamed up to transform the KNVB Campus in Zeist – the beating heart of Dutch football.

Optimizing a Hoog Op Tennis Club’s lighting

Signify Certified System Integrator, Oostendorp Nederland, delivered an innovative, connected lighting solution to enhance the member experience at Hoog Op Tennis Club.

Grand Stade de Tanger by Lamalif

The Ibn Batouta Stadium in tangier stands as a true showcase of Signify’s cutting-edge lighting technology. Featuring Arenavision with BVP428 luminaires for the pitch and ClearFlood BVP650 for the stands, and Unistrip BCP383 for the façade. The stadium delivers unmatched visibility, safety, and ambiance for players and fans alike. This state-of-the-art system positions the venue at the forefront of global sports infrastructure, ready to shine brilliantly for AFCON 2025, the 2030 World Cup, and millions of passionate fans across the continent.

Ekinox Arena

Philips ArenaVision LED sports lighting in Ekinox Arena

Lacrosové hřiště Radotín

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Smart office lighting – Arrival

Bus operator Arriva achieved complete control over their lighting and reduced energy usage thanks to Interact Pro.

Sevens Stadium - UAE

Lighting the future of sport with sustainability in every kick

A focus on fan experience and new revenue streams – Optus Stadium

With the goal of creating the ultimate fan experience, the recent all-LED lighting and Interact Sports software at Optus Stadium makes it the premier multipurpose venue in the Southern Hemisphere.

Smart lighting for best multipurpose arena experience – Buesa Arena

The Fernando Buesa Arena in Spain converted 100% of the lighting to LED and connected via a standard wired connection, all remotely controlled and managed with Interact Sports.

Fan experience and easy control – Allianz Stadium

Interact Sports offers an easy-to-use dashboard to control all the lighting systems in Allianz Stadium. Allianz now enjoys increased fan engagement, high-quality broadcast capabilities and new revenue potential.

Melbourne Cricket Ground by Lightmoves

The Melbourne Cricket Ground (MCG), a 100,000 person stadium in Melbourne, hosts major international, national, and local sporting events and concerts, including the Boxing Day Test, AFL Grand Final, and performances by artists such as AC/DC and Taylor Swift. The project involved retrofitting 12 electrical zones across 7 levels, replacing the legacy control system with a Dynalite solution to deliver enhanced, venue-wide control.

Connected stadium – fan experience

As Turkey’s largest multipurpose venue, the Sinan Erdem Arena has installed Interact Sports management software to bring a connected stadium concept to life using connected LED lighting infrastructure.

Starting a project?

Starting a project?

We’d love to hear from you.