Vukovar promenade Croatia

Vukovar promenade Croatia

By Lipapromet

Vukovar promenade Croatia

Promenade along the Drava River - Magic Forest

Vukovar, Croatia

A centuries-old mixed forest bordered by the wetlands of the Vuka River has been brought to life using dynamic lighting to illuminate the treetops.

Challenge

Customer challenge

The municipality wanted to strengthen Vukovar's tourist offer and present the natural beauty of the promenade along the Vuka River, while also attracting tourists also at night.

Solution

The solution

High-quality RGBW lighting fixtures were installed on trees using non-invasive installation accessorie in order to preserve living trees. A careful arrangement of lighting fixtures and dynamic scenes was implemented which slightly changes the color or color combinations of individual treetops, creating a calming experience for the observer. Walking along a wooden path above the floodplains of the Vuka River in the midst of silence and darkness, the visitor is shown impressive structures of illuminated trees and branches.

Team

Certified System Integrator: Lipapromet d.o.o.

Lighting Designer: Diana Galić, NOVA-LUX d.o.o.

Client / end user: Vukovar

Products

Color Kinetics ColorBurst

Color Kinetics iPlayer3

Discover other case studies

Federation Square by bluebottle

bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.

A sustainably designed city – Gaiserwald, Switzerland

IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.

Joint vision brings smart lighting to citizens – Rogaland, Norway

Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.

Smart Street Lighting NY and Interact

NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.

Illuminating London's bridges for the world’s longest public art commission

Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.

A small city lighting the way with connected street lighting – Ribeira, Spain

Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.

Solar Streelighting at Falcon City of Wonders, Dubai

Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.

Sheffield Tramline

Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps

Municipalities of Veneto

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Public lighting renewal in Roztoky

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Creating a vibrant city center – Smart Lighting

The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.

Ningbo, China enhances its skyline with connected LED lighting

Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.

Starting a project?

Starting a project?

We’d love to hear from you.