Ribeira at the cutting edge of connected LED lighting
Ribeira at the cutting edge of connected LED lighting

Ribeira at the cutting edge of connected LED lighting

Ribeira

Spain

The Ribeira Council in Spain replaced around 8,600 urban light points with LED luminaires, 6,500 of which are controlled and managed via Interact City, putting Ribeira at the cutting edge of public lighting in Europe.

“The investment in Interact City was spurred by the technological capabilities of the system. It’s an innovative tool with a lot of potential to integrate new services. It’s also scalable and can help a city become 'smart'.”

- Alejandro García Sendón, Technical and Energy Services Coordinator of Ferrovial Servicios for the north of Spain

Customer Challenge

Ribeira’s Municipal Corporation had two major objectives: to improve energy efficiency and to create well-lit spaces so people feel safer at night. To achieve this, they needed to renew an urban lighting network comprising over 8,600 light points. The new connected LED luminaires are controlled and managed by Interact City software. By reducing energy consumption and streamlining maintence, the city can invest cost savings in other areas of their smart city project.

Hassle-free connected lighting

 

“One of the great things about Interact City is how much time and hassle it saves. Because it’s a plug-and-play system, the set-up is so quick and easy. Commissioning is taken care of automatically – all it takes is one click,” says Jose da Torre, Maintenance and Works Manager for Ribeira Ferrovial Servicios.

 

With Interact City Lighitng asset management, as soon as the luminaire connects to Interact City, it’s ready for operation, with all the data from the road lighting automatically appearing on an easy-to-use interface. The luminaire immediately begins relaying performance data, including lighting levels and energy consumption.

 

With Interact City Scene management, luminaires can be controlled individually or in groups, either in near realime or pre-scheduled. This way, varying light levels can be delivered throughout the city, depending on need.

 

“Interact City makes managing lighting much easier,” adds da Torre. “We can experiment with the lighting until we get the right level for each environment. And if there’s an incident, we can adjust the lighting immediately.”

 

 

Discover other case studies

Federation Square by bluebottle

bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.

A sustainably designed city – Gaiserwald, Switzerland

IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.

Joint vision brings smart lighting to citizens – Rogaland, Norway

Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.

Smart Street Lighting NY and Interact

NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.

Illuminating London's bridges for the world’s longest public art commission

Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.

Solar Streelighting at Falcon City of Wonders, Dubai

Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.

Sheffield Tramline

Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps

Municipalities of Veneto

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Public lighting renewal in Roztoky

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Creating a vibrant city center – Smart Lighting

The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.

Ningbo, China enhances its skyline with connected LED lighting

Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.

Starting a project?

Starting a project?

We’d love to hear from you.