A united vision on smart street lighting
A united vision on smart street lighting

A united vision on smart street lighting

Rogaland County

Norway

In Rogaland, Norway, 18,000 connected LED street lights, which are managed and controlled by Interact City software, have been installed across eleven municipalities, as part of a two-year plan to become a smart municipality.

“Being able to control each individual light point is a very valuable feature. We can turn up the brightness in a neighborhood where more light is required, and we can turn it down in other areas when not needed.”

- Jarl Hoogstad, Product Manager for road and street lighting at Lyse Elnett

Customer challenge

Eleven towns in the Rogaland region came together in a united effort to upgrade their city infrastructure and enable smart technologies to improve life for their citizens. The recently installed connected LED street lighting is just the first step in a two-year plan to roll out smart technologies, including sensors and other connected devices. The region’s goals are to improve operational efficiency, reduce costs and improve the livability cities for citizens.

Central control of all connected light points

 

Lyse Elnett, an industrial company owned by the municipalities in Rogaland, initiated this large-scale road and street lighting upgrade and is managing the project. Some municipalities have also included lighting for parks and footpaths.

 

"Stavanger municipality wanted to expand the project to include upgrading park lighting as well as street lighting. The park lighting is controlled via Interact City in the same way as the street lighting. We can do this for all exterior lighting, and this is in keeping with our thinking about smart lighting control. Being able to control each individual light fixture is a very valuable feature. We can turn up the brightness in a neighborhood where more light is required, and conversely we can turn it down in other areas when not needed," says Jarl Hoogstad, Product Manager for road and street lighting at Lyse Elnett.

 

The solution offers great benefits to both users and operators. Interact City is easy to operate via a centralized dashboard at Lyse Elnett or locally at each of the municipalities, and Lighting asset management software provides an interactive map that shows the location and status of all the network’s light points. The system also sends an immediate error message in case of a lighting fault, ensuring a quick and accurate maintenance response.

 

Interact City Scene management software offers Rogaland’s municipalities simple and shared control over a large number of light points. Authorized users can manage individual lights or create zones, increasing brightness in certain neighborhoods while dimming in areas that are not in use.

 

The municipalities are also thinking ahead. With an open systems approach, Intearct City is scalable and future ready for new IoT applications enabled by sensors and other smart city functionality.

Discover other case studies

Federation Square by bluebottle

bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.

A sustainably designed city – Gaiserwald, Switzerland

IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.

Smart Street Lighting NY and Interact

NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.

Illuminating London's bridges for the world’s longest public art commission

Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.

A small city lighting the way with connected street lighting – Ribeira, Spain

Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.

Solar Streelighting at Falcon City of Wonders, Dubai

Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.

Sheffield Tramline

Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps

Municipalities of Veneto

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Public lighting renewal in Roztoky

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Creating a vibrant city center – Smart Lighting

The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.

Ningbo, China enhances its skyline with connected LED lighting

Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.

Starting a project?

Starting a project?

We’d love to hear from you.