Heineken Diamond Corner

The Diamond - Heineken Hoek

By Livingprojects

Heineken Diamond Corner Daylight

The Diamond – Heineken Hoek

Amsterdam

This project is a prime example of co-creation. In close collaboration with MVSA Architects and Octatube, every choice—from light color (cool white, 4000K) to placement—was meticulously crafted. Using mock-ups, lighting calculations, and practical tests, a lighting scheme was created that optimally showcases the diamond facade, without any annoying reflections or the familiar "zebra crossing effect."

 

The renovated Heineken Hoek demonstrates how architecture, light, and technology can merge into a comprehensive visual experience. From A to WOW. Anyone walking across Leidseplein today will agree: this diamond sparkles brighter than ever.

Heineken Diamond Corner Dark

Customer challenge

The Heineken Hoek has been a landmark on Leidseplein for decades. Yet, the iconic location was in need of a fresh impetus. Livingprojects was involved from the outset to create a lighting design that enhances the layered architecture without being overpowering.

Heineken Diamond Corner Lighting zoom

The solution

Commissioned by Heineken Nederland and Caransa Groep, MVSA Architects designed a completely new building with a bold, contemporary character. Featuring a transparent Octatube curtain wall, six stories, a glass canopy, and a façade that subtly references the famous Koh-i-Noor diamond, The Diamond is not only a four-star hotel but also an ode to Amsterdam's diamond heritage. A subtle yet powerful lighting solution that illuminates the glass facade from within. Invisibly placed, without distracting elements, and fully tailored to the comfort of hotel guests. The light should shine, not disturb. Therefore, Livingprojects opted for a solution that was not only aesthetically pleasing but also created a sense of tranquility in the hotel rooms.

Team

Certified System Integrator: Livingprojects

Lighting Designer: Nick Dankers

Client / end user: Heineken Netherlands / Caranza Group

Architect: MVSA Architects

Products

140x BCP386 60LED 40K 24V A11 L100 DMX

21x BCP386 30LED 40K 24V A11 L50 DMX

17x BCP386 12LED 40K 24V A11 L30 DMX

Discover other case studies

Megarex Haguenau by CGR/ICE theaters

This is a world first: it’s the very first cinema screen that combines a giant LED display (instead of a traditional projector screen) with CGR Cinemas’ ICE Theaters technology, which uses Signify’s LightVibes system.

Intelligent lighting - Hotel Rosewood Villa Magna, Interact

The Rosewood Villa Magna hotel has been comprehensively renovated to become the highest quality, most luxurious, and most exclusive hotel in Madrid.

Fairmont Ramla Riyadh

Seamless lighting control and guest room management courtesy of Signify

Mondrian Gold Coast by Bluebottle

At Mondrian Gold Coast, a new landmark on Burleigh Beach, bluebottle delivered an integrated GRMS using Signify’s Dynalite and Interact for Hospitality. The system unifies lighting, HVAC, occupancy, and room controls across guest areas and the public realm, boosting comfort, efficiency, and real-time management.

Meryal Water Park by Zeeman Services and Solutions WLL

23 building with DALI based lighting control system and 5 different zones site wide DMX based lighting control system with central driver solution.

Swissotel The Stamford

With Interact Hospitality, Swissotel The Stamford in Singapore can personalize the guest experience while increasing staff efficiency, saving energy, and meeting sustainability goals.

The Cultural Centre Spira by Kreativ Teknik

During the autumn, Kreativ Teknik completed a project together with Elektrobyrån and Signify at Cultural Centre Spira in Jönköping. The upper parts of the facade received a new lighting design and illumination and were programmed with beautiful scenarios.

Dynamic light shows create a night to remember

Novotel Da Nang chose Interact Hospitality connected lighting to deliver striking light shows, transforming the hotel facade in to an after-dark landmark.

Hotel Pillows Anna van den Vondel

Interact and Certified System Integrator Tovèrli Lighting & Control Solutions teamed up to transform guest services in Hotel Pillows Anna van den Vondel Amsterdam.

Flight Club by bluebottle

bluebottle has delivered multiple Flight Club venues across Australia, bringing its dynamic social darts experience to life. We implemented a control system using Signify's Dynalite integrated with Pharos, plus custom integration to dartboards, enabling reactive lighting effects that sync with gameplay, sound, and ambient shifts—elevating the venue’s playful, immersive atmosphere.

NatureConnect Transforms Grieghallen

Grieghallen chose Signify’s NatureConnect solution and NatureConnect boosts mood and energy in a former shelter.

Starting a project?

Starting a project?

We’d love to hear from you.