Meryal Water Park

Meryal Water Park

By Zeeman Services and Solutions WLL

Meryal Water Park

Meryal Water Park at Qateifan Island

Doha, Qatar

Meryal Water Park is the largest water park spread over 6 acres with 56 slides including world's tallest waterslide. This complex project focused on equiping 23 buildings with a complete centralised DALI based lighting control system, the installation of a side wide outdoor DMS control system in 5 different zones and a central driver solution installed in 25 different feeder pillar locations  for sitewide control  with central PC and BMS integration.

Challenge

Customer challenge

The major challenge in the project was to provide a central driver solution to drive the LED from the Central feeder pillar location.Redesign the complete load schedule based on the controller/central driver rating and recommending the cable size based on the voltage drop calculation to connect the different types of LED load.

Solution

The solution

The project contains many technically advanced features. It includes a centralized Lighting control system for 23 buildings with DALI multi function sensors, manual override control, time scheduling for multiple scenes, BMS and FAS integration. A site wide DMX based lighting control system with 5 different zones is installed with 5 different networks with multiple feeder pillars with central driver to operate the filed level LED's through 24V dc power. It offers an interface to the rides control system,BMS and FAS.

Team

Certified System Integrator: Zeeman Services and Solutions WLL

Lighting Designer: Atkins/Aurecon

Client / end user: Qateifan Projects

Main Contractor: Redco Almana

Products

iLight DALI system 

Zeros DMX Server

Discover other case studies

Megarex Haguenau by CGR/ICE theaters

This is a world first: it’s the very first cinema screen that combines a giant LED display (instead of a traditional projector screen) with CGR Cinemas’ ICE Theaters technology, which uses Signify’s LightVibes system.

Intelligent lighting - Hotel Rosewood Villa Magna, Interact

The Rosewood Villa Magna hotel has been comprehensively renovated to become the highest quality, most luxurious, and most exclusive hotel in Madrid.

Fairmont Ramla Riyadh

Seamless lighting control and guest room management courtesy of Signify

The Diamond - Heineken Hoek by Livingprojects

The renovated Heineken Hoek demonstrates how architecture, light, and technology can merge into a comprehensive visual experience.

Mondrian Gold Coast by Bluebottle

At Mondrian Gold Coast, a new landmark on Burleigh Beach, bluebottle delivered an integrated GRMS using Signify’s Dynalite and Interact for Hospitality. The system unifies lighting, HVAC, occupancy, and room controls across guest areas and the public realm, boosting comfort, efficiency, and real-time management.

Swissotel The Stamford

With Interact Hospitality, Swissotel The Stamford in Singapore can personalize the guest experience while increasing staff efficiency, saving energy, and meeting sustainability goals.

The Cultural Centre Spira by Kreativ Teknik

During the autumn, Kreativ Teknik completed a project together with Elektrobyrån and Signify at Cultural Centre Spira in Jönköping. The upper parts of the facade received a new lighting design and illumination and were programmed with beautiful scenarios.

Dynamic light shows create a night to remember

Novotel Da Nang chose Interact Hospitality connected lighting to deliver striking light shows, transforming the hotel facade in to an after-dark landmark.

Hotel Pillows Anna van den Vondel

Interact and Certified System Integrator Tovèrli Lighting & Control Solutions teamed up to transform guest services in Hotel Pillows Anna van den Vondel Amsterdam.

Flight Club by bluebottle

bluebottle has delivered multiple Flight Club venues across Australia, bringing its dynamic social darts experience to life. We implemented a control system using Signify's Dynalite integrated with Pharos, plus custom integration to dartboards, enabling reactive lighting effects that sync with gameplay, sound, and ambient shifts—elevating the venue’s playful, immersive atmosphere.

NatureConnect Transforms Grieghallen

Grieghallen chose Signify’s NatureConnect solution and NatureConnect boosts mood and energy in a former shelter.

Starting a project?

Starting a project?

We’d love to hear from you.