Enhancing guest experience at Swissotel The Stamford
Enhancing guest experience at Swissotel The Stamford

Enhancing guest experience at Swissotel The Stamford

Swissotel The Stamford

Singapore

Swissotel, in Singapore, is committed to providing an outstanding guest experience and enhancing employee satisfaction with smart room control technology while maximizing operational and energy efficiencies.

“Interact Hospitality has helped us strengthen our brand pillar of enhancing employee satisfaction, which has in turn enhanced guest satisfaction.”

- Katya Herting, Hotel Manager, Swissotel The Stamford

Customer challenge

The 1,261-room five-star hotel, part of the Accor group, is one of the tallest in Southeast Asia at 226 meters high. With a firm commitment to providing an enhanced guest experience and meeting sustainability goals, Swissotel was looking for a system that would help improve staff efficiency and seamlessly integrate with other automated hospitality systems such as HVAC and Oracle Opera. Interact Hospitality was the answer.

Enhancing guest experiences and improving hotel operations

 

The superior guest experience starts upon arrival at the front desk, according to Nicolas Mak, Director of Facilities at Swissotel The Stamford. When guests check in, the air conditioning will be set at an optimum temperature. Sensors in the room detect when guests have arrived in the room and the lights will turn on. The automated communication between systems maximizes energy efficiency and improves the guest experience, while helping Swissotel meet their sustainability goals.

Once guests are in their hotel room, they can use a single control panel to select their desired lighting scene and room temperature. The lighting scenes provide a warm welcome upon arrival in the room, and also help guest unwind in the evening with a relaxing scene.

Dynamic in-room night lighting sensors respond when guests rise during the night, with low level lighting illuminating the floor automatically for increased safety. And because 35% of people leave the light on in the bathroom during the night, which negatively affects deep sleep, automated lighting helps guest enjoy a better night’s sleep.

The Interact Hospitality dashboard allows staff to see real-time guest requests, ensuring quick response and turnaround times, helping to improve productivity and service levels. With a single touch, guests can activate a ‘pick up my laundry’ request from the room, which feeds into a central dashboard to notify that the room does need to be visited. According to Katya Herting, Hotel Manager, “We have significantly improved the time it takes between a guest pressing the button for laundry pick up and the runner to pick up the laundry.” The system also reduces unnecessary work for staff while minimizing guest disruption, resulting in an overall increase in customer and staff satisfaction.

The new system is fully customizable and seamlessly integrates with third-party systems such as heating, ventilation and air conditioning (HVAC), sharing real-time information about the guest room. Occupancy insights from the sensors help lower energy consumption by adjusting heating and cooling levels when rooms are unoccupied.

The Interact Hospitality system reinforces the hotel’s reputation for comfort, elegance and style. It also supports Swissotel’s commitment to delivering outstanding guest experiences in an energy-efficient, sustainable way.

Discover other case studies

Megarex Haguenau by CGR/ICE theaters

This is a world first: it’s the very first cinema screen that combines a giant LED display (instead of a traditional projector screen) with CGR Cinemas’ ICE Theaters technology, which uses Signify’s LightVibes system.

Intelligent lighting - Hotel Rosewood Villa Magna, Interact

The Rosewood Villa Magna hotel has been comprehensively renovated to become the highest quality, most luxurious, and most exclusive hotel in Madrid.

Fairmont Ramla Riyadh

Seamless lighting control and guest room management courtesy of Signify

The Diamond - Heineken Hoek by Livingprojects

The renovated Heineken Hoek demonstrates how architecture, light, and technology can merge into a comprehensive visual experience.

Mondrian Gold Coast by Bluebottle

At Mondrian Gold Coast, a new landmark on Burleigh Beach, bluebottle delivered an integrated GRMS using Signify’s Dynalite and Interact for Hospitality. The system unifies lighting, HVAC, occupancy, and room controls across guest areas and the public realm, boosting comfort, efficiency, and real-time management.

Meryal Water Park by Zeeman Services and Solutions WLL

23 building with DALI based lighting control system and 5 different zones site wide DMX based lighting control system with central driver solution.

The Cultural Centre Spira by Kreativ Teknik

During the autumn, Kreativ Teknik completed a project together with Elektrobyrån and Signify at Cultural Centre Spira in Jönköping. The upper parts of the facade received a new lighting design and illumination and were programmed with beautiful scenarios.

Dynamic light shows create a night to remember

Novotel Da Nang chose Interact Hospitality connected lighting to deliver striking light shows, transforming the hotel facade in to an after-dark landmark.

Hotel Pillows Anna van den Vondel

Interact and Certified System Integrator Tovèrli Lighting & Control Solutions teamed up to transform guest services in Hotel Pillows Anna van den Vondel Amsterdam.

Flight Club by bluebottle

bluebottle has delivered multiple Flight Club venues across Australia, bringing its dynamic social darts experience to life. We implemented a control system using Signify's Dynalite integrated with Pharos, plus custom integration to dartboards, enabling reactive lighting effects that sync with gameplay, sound, and ambient shifts—elevating the venue’s playful, immersive atmosphere.

NatureConnect Transforms Grieghallen

Grieghallen chose Signify’s NatureConnect solution and NatureConnect boosts mood and energy in a former shelter.

Starting a project?

Starting a project?

We’d love to hear from you.