Rams Park Galatasaray Stadium

Rams Park Galatasaray Stadium

By Şah Eletrkik Aydınlatma

Rams Park Galatasaray Stadium Façade and Ambiance Lighting

Istanbul, Turkey

The project has two main components. Indoors, the grandstand roof was integrated with the sound system and illuminated dynamically in team colors, boosting fan excitement and engagement. On the exterior façade, synchronized dynamic lighting creates a visual show on match days and throughout the week, turning the stadium into a striking evening landmark.

“The new Philips and DMX lighting system dramatically elevated our match-day atmosphere, so much so that even Liverpool’s delegation praised its impact."

 

Director of Stadium Operations , Galatasaray Sports Club

Challenge

Customer challenge

Galatasaray needed to upgrade its lighting system to enhance the match atmosphere, boost fan engagement, and create a more striking night-time appearance. The existing infrastructure did not support dynamic color changes, digital control, or scenario-based ambience. The club sought a new solution compatible with Signify’s high-tech, smart automation platform to deliver impactful visual experiences across both the stands and the façade.

Solution

The solution

We delivered a fully dynamic lighting solution using color-changing Philips luminaires and DMX-based digital control, enabling synchronized scenarios across the façade and grandstands. The new system strengthens the match-day atmosphere, boosts fan engagement, and enhances the stadium’s night-time identity. Powered by Signify’s reliable, high-tech platform, the venue now offers a unique and immersive visual experience.

Team

Certified System Integrator: Şah Aydınlatma - Oğuzhan Keçeci 

Lighting Designer: Kerem Akgün, İrem Bekar, Olcay Karamusaoğlu

Client / end user: Galatasaray Sports Club

Optional other teams: Mehmet Akif Tandoğru, Tuğba Kuzyaka

Products

BVP355 216LED RGBW57K220VL57 10/15/30DMX

BVP353 72LED RGBW57K 220V L57 30 DMX

BCS342 120LED RGBWW 24V OC L100 DMX

BCS342 60LED RGBWW 24V OC L50 DMX

BCS342 36LED RGBWW 24V OC L30 DMX

BVP355 216LED RGBWW 220V L57 30 DMX

BVP354 144LED RGBWW 220V L57 60 DMX

BVP355 216LEDRGBW57K 220V L57 45 DMX MSP

BVP355 216LEDRGBW57K 220V L57 45 DMX

ZXP399 Lead 4P DMX cable 2m (10 pcs)

ZXP399 Jump 4P DMX cable 2m (10 pcs)

ZXP399 Jump 4P DMX cable 5m (10 pcs)

ZXP399 endcap female connector (20 pcs)

ZXP399 DMX amplifier 24V 4P

ZXP399 Addressing Kit DMX

ZXP399 Lead 5P DC/DMX cable 2m (10 pcs)

ZXP399 Jump 5P DC/DMX cable 2m (10 pcs)

ZXP399 Y-connect kit 5P DC/DMX (10 pcs)

ZXP399 Jump 5P DMX connector (10 pcs)

ZXP399 DMX amplifier 24V 5P

LED Transformer 150W IP67 24VDC 220-240V

ZXP399 sub-controller 12V 16 port DMX

Discover other case studies

The KNVB Campus - Zeist, The Netherlands

Interact and Certified System Integrator Oostendorp Nederland B.V. teamed up to transform the KNVB Campus in Zeist – the beating heart of Dutch football.

Optimizing a Hoog Op Tennis Club’s lighting

Signify Certified System Integrator, Oostendorp Nederland, delivered an innovative, connected lighting solution to enhance the member experience at Hoog Op Tennis Club.

Grand Stade de Tanger by Lamalif

The Ibn Batouta Stadium in tangier stands as a true showcase of Signify’s cutting-edge lighting technology. Featuring Arenavision with BVP428 luminaires for the pitch and ClearFlood BVP650 for the stands, and Unistrip BCP383 for the façade. The stadium delivers unmatched visibility, safety, and ambiance for players and fans alike. This state-of-the-art system positions the venue at the forefront of global sports infrastructure, ready to shine brilliantly for AFCON 2025, the 2030 World Cup, and millions of passionate fans across the continent.

Ekinox Arena

Philips ArenaVision LED sports lighting in Ekinox Arena

Megarex Haguenau by CGR/ICE theaters

This is a world first: it’s the very first cinema screen that combines a giant LED display (instead of a traditional projector screen) with CGR Cinemas’ ICE Theaters technology, which uses Signify’s LightVibes system.

Lacrosové hřiště Radotín

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Smart office lighting – Arrival

Bus operator Arriva achieved complete control over their lighting and reduced energy usage thanks to Interact Pro.

Sevens Stadium - UAE

Lighting the future of sport with sustainability in every kick

A focus on fan experience and new revenue streams – Optus Stadium

With the goal of creating the ultimate fan experience, the recent all-LED lighting and Interact Sports software at Optus Stadium makes it the premier multipurpose venue in the Southern Hemisphere.

Smart lighting for best multipurpose arena experience – Buesa Arena

The Fernando Buesa Arena in Spain converted 100% of the lighting to LED and connected via a standard wired connection, all remotely controlled and managed with Interact Sports.

Fan experience and easy control – Allianz Stadium

Interact Sports offers an easy-to-use dashboard to control all the lighting systems in Allianz Stadium. Allianz now enjoys increased fan engagement, high-quality broadcast capabilities and new revenue potential.

Intelligent lighting - Hotel Rosewood Villa Magna, Interact

The Rosewood Villa Magna hotel has been comprehensively renovated to become the highest quality, most luxurious, and most exclusive hotel in Madrid.

Starting a project?

Starting a project?

We’d love to hear from you.