City of Grenchen

City of Grenchen

By Elektron AG

City of Grenchen

Upgrade instead of replace: Circular lighting meets Interact City

Grenchen / Switzerland

ELEKTRON AG and Signify realized Switzerland’s first circular luminaires "Luma gen1 UP" connected to Interact City. Existing luminaires were upgraded to state-of-the-art technique including Zhaga-connectivity, instead of replacing them: Saving 76% CO₂ and valuable materials. The city now monitors and controls both new and circular luminaires in Interact City, saving energy and maintenance costs while achieving its sustainability goals.

Heide Smale snapshot

 

“All our luminaires – new or circularly upgraded first-generation Luma – are now connected, controlled and monitored via Interact City.”


Andreas Messerli
Head of Operations and Maintenance, SWG

City of Grenchen - Challenge

Customer challenge

Until now, luminaires in public lighting were used linearly and disposed of at end of life. ELEKTRON AG aimed to change this by providing a refurbishment service including a connectivity upgrade to Interact City, together with its first mover customer in Grenchen. The goal: Use materials sustainably, reduce CO₂ emissions, and increase energy and maintenance efficiency. The challenge was to connect both new and upgraded luminaires in Interact City.

City of Grenchen - Solution

The solution

Signify's first generation of Luma luminaires were circularly upgraded in Switzerland by a social institution. The housings were reused and equipped with a Signify upgrade kit, saving around 76% CO₂ compared to producing new ones. On top, each luminaire now includes two Zhaga interfaces for seamless integration into Interact City, enabling smart control, 30% energy savings, and major efficiency gains in daily operation. Additionally, light color changed from 4000K to 3000K to meet modern street lighting standards.

Team

Certified System Integrator: ELEKTRON AG

Lighting Designer: ELEKTRON AG

Client / end user: Stadtwerke Grenchen SWG

Products

Luma Gen1 Luminaires (from 2015-2017 to be refurbished)

Luma Gen1 Upgrade Kit

Zhaga OLC & Signify Interact City Software

Discover other case studies

Federation Square by bluebottle

bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.

A sustainably designed city – Gaiserwald, Switzerland

IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.

Joint vision brings smart lighting to citizens – Rogaland, Norway

Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.

Smart Street Lighting NY and Interact

NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.

Illuminating London's bridges for the world’s longest public art commission

Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.

A small city lighting the way with connected street lighting – Ribeira, Spain

Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.

Solar Streelighting at Falcon City of Wonders, Dubai

Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.

Sheffield Tramline

Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps

Municipalities of Veneto

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Public lighting renewal in Roztoky

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Creating a vibrant city center – Smart Lighting

The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.

Ningbo, China enhances its skyline with connected LED lighting

Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.

Starting a project?

Starting a project?

We’d love to hear from you.