Brașov City

Brașov City

By Flash Lighting Services SA

Brașov City

Full city-wide LED installation

Brasov City, Romania

Brașov City continues its investment program in efficient public lighting solutions and is replacing all classic sodium lighting fixtures with LED lighting fixtures on streets where this system does not yet exist, in order to switch to 100% LED lighting.

 

Thus, in addition to the 8,200 existing LED public lighting systems, the municipality has begun installing another 8,425 such systems.

 

In addition, the entire lighting system on the city streets will be equipped with a remote management system, which will allow efficient control of the public lighting operation and rapid identification of malfunctions.

“We have managed to implement the project to increase the efficiency of public lighting by replacing classic sodium lighting fixtures with LED lamps, which are more economical, more efficient, and can be adjusted through the remote management system. We were able to complete this project and, in this way, Brașov will practically have 100% modern LED lighting. In short, we can say that we have taken a very important step in terms of energy efficiency and reducing energy bills. We are among the few cities in Romania that have managed to reach this level."

 

George SCRIPCARU, 
Mayor of Brasov City

Challenge

Customer challenge

The energy consumed by the public lighting infrastructure in a city accounts for up to 40% of the total energy consumed by the municipality, so the urge to do real savings is more real than ever. Also, in a time dominated by IoT solutions, the old generation of luminaires such as Sodium High Pressure Lamps are old news. So a solution to really reduce energy costs, but also to improve the availability of the public lighting system using modern smart lighting control and monitoring software was necessary.

 

Another element that was taken into consideration, the quality of lighting provided to the citizens, coming from the appropriate light temperature, going to the right amount of light in the streets and closing with the uniformity of the illumination.

Solution

The solution

The energy efficiency project that we are implementing in the municipality of Brașov is one of the largest projects implemented in Romania. It involves replacing 8,425 lighting fixtures with modern LED lighting fixtures equipped with a remote management system. This system allows the control of each lighting fixture individually. It collects data on the operating parameters of the lighting fixture and can receive commands regarding switching on, off, and possibly dimming (increasing or decreasing the light intensity, n.n.) for each lighting fixture through the remote management platform, which is managed by the dispatcher. We receive alerts for each lighting fixture if it is functional, if it breaks down, etc. By replacing these 8,425 lighting fixtures, the system produces a saving of 60%, which, in monetary terms, brings savings to the municipality’s budget of approximately €0.5 million annually.

Team

Certified System Integrator: FLASH LIGHTING SERVICES SA

Lighting Designer: Mihai Pencea / Tiberiu Nicolaev

Client / end user: BRASOV MUNICIPALITY

Other teams: Andrei Opincaru Technical Manager, George Zaharia R&D Department, Ioan Preda Execution Department, Cristian Ghilt Project Manager

Products

Signify Luminaires 

BGP281I BGP281 LWCO LED70-1P/730 I DN11P FG-AR I

BGP281I BGP281 LWCO LED109-1P/730 I DM24P FG-AR 

BGP282I BGP282 LWCO LED210-1P/730 I DN08P FG-AR

 

Signify outdoor lighting controllers   

SW913705000248 Interact City Vf EU-US ,

LLC7852/00 CT NODE ZHAGA DC EU4VF LG

 

Signify multisensor

Discover other case studies

Federation Square by bluebottle

bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.

A sustainably designed city – Gaiserwald, Switzerland

IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.

Joint vision brings smart lighting to citizens – Rogaland, Norway

Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.

Smart Street Lighting NY and Interact

NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.

Illuminating London's bridges for the world’s longest public art commission

Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.

A small city lighting the way with connected street lighting – Ribeira, Spain

Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.

Solar Streelighting at Falcon City of Wonders, Dubai

Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.

Sheffield Tramline

Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps

Municipalities of Veneto

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Public lighting renewal in Roztoky

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Creating a vibrant city center – Smart Lighting

The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.

Ningbo, China enhances its skyline with connected LED lighting

Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.

Starting a project?

Starting a project?

We’d love to hear from you.