The Wallonia region of Belgium is located at the crossroads of various major European arterial roads, making its road network important for the economic development of the European Union (EU).
Wallonia
Wallonia, Belgium
Our regional lighting budget is unchanged. But we now have more efficient and environmentally friendly lighting, because it is recyclable, and therefore more sustainable.”
- Denis Cornet, Manager Mobility and Infrastructure SPW
Customer challenge
For SOFICO, the Walloon infrastructure financing company responsible for managing Wallonia’s motorways and main roads, the highest priorities for Wallonia's road network were safety, sustainability, and cost. The company needed to ensure that Wallonia possessed a safe road network with a steady flow and a sustainable lighting network to operate in line with European climate goals.
Solution
The Lumières 4.0 plan, the result of a public-private partnership between SOFICO and the LuWa consortium, provides intelligent LED lighting across a 2,700km stretch of motorways—all controlled by an Interact connected lighting system from Signify.
To guarantee its lighting solution was sustainable, Signify proposed using its new circular LED luminaires from Philips. Because all components of these luminaires can be reused at the end of their service life, they were the best choice both economically and ecologically, not to mention the fact that their circular design makes them easier to repair.
The lighting on each route is controlled from the Perex traffic centre near Namur, Belgium, and adjusted based on traffic, weather conditions, accidents, road construction, and repairs. Interact automatically and immediately sends data-rich alerts regarding system outages or interruptions in service, as well as using real-time performance data to assess when luminaires are likely to need replacing, allowing for preventive maintenance. This limits the need for hazardous roadside work, improving safety for maintenance workers.
The connected LED luminaires paired with Interact contribute to a 76% reduction in electricity consumption. For SOFICO, that means a significant reduction in operating costs. This reduction allows the region to recoup its investment. Meanwhile, the energy savings will result in a reduction of 166,000 tons of CO₂ emissions over 20 years.
Discover other case studies
Federation Square by bluebottle
bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.
A sustainably designed city – Gaiserwald, Switzerland
IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.
Joint vision brings smart lighting to citizens – Rogaland, Norway
Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.
Smart Street Lighting NY and Interact
NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.
Illuminating London's bridges for the world’s longest public art commission
Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.
A small city lighting the way with connected street lighting – Ribeira, Spain
Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.
Solar Streelighting at Falcon City of Wonders, Dubai
Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.
Sheffield Tramline
Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps
Municipalities of Veneto
Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.
Public lighting renewal in Roztoky
Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.
Creating a vibrant city center – Smart Lighting
The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.
Ningbo, China enhances its skyline with connected LED lighting
Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.
Starting a project?
We’d love to hear from you.