Sodium street lights were removed from the center of Szczecin, Poland and replaced with energy-efficient LED lighting. In total, almost 5,000 Philips Luma LED luminaires were installed, 1,888 of which are managed by Interact City Lighting asset management and Scene management software.
Szczecin
Poland
“Interact City provides a high level of flexibility to meet the different lighting needs in our city at any time.”
- Radoslaw Tumielewicz, Director of Roads and Transport Authority, Szczecin
Customer Challenge
Szczecin aims to be an attractive city for investors and tourists, as well as a safe and friendly city for its citizens.
To enhance its attractiveness and competitiveness, the city’s municipal authorities raised funding under the energy-efficient street lighting priority program of the Green Investment Scheme (GIS) in Poland, aimed at replacing existing street lighting with a modern, eco-friendly, and economical system.
Hassle-free connected lighting
Szczecin is the seventh most populous city in Poland, with over 400,000 residents. A center of the country’s maritime economy, the north western city handles shipping from around the world. Because the downtown area is filled with greenery and rivers, Szczecin is nicknamed the ‘Floating Garden’ and it wants to build on its reputation as an attractive place for investors and tourists, as well as a safe and friendly city for its citizens.
Energy-efficient LED luminaires, combined with Interact City software, were selected for the project. With centralized communication and control of individual light points, the network was transformed into a smart lighting system. With Interact City Scene management, individual luminaires can be switched on and off, or dimmed to a specific lighting level, on an ad hoc basis, or according to a daily or seasonal calendar.
Interact City lighting asset management software delivers valuable information on each luminaire’s status and energy use, while automatically sending fault notifications in case of an outage. Altogether, the connected street lighting system provides cost savings of up to 70%, contributing significantly to Szczecin’s smart city approach. With no expensive ‘scouting’ for luminaire outages, both energy and maintenance costs are significantly reduced, improving the overall management of the city’s lighting. If luminaires do fail, the maintenance crews can be notified immediately, improving efficiency as well as lighting standards.
Discover other case studies
Federation Square by bluebottle
bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.
A sustainably designed city – Gaiserwald, Switzerland
IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.
Joint vision brings smart lighting to citizens – Rogaland, Norway
Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.
Smart Street Lighting NY and Interact
NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.
Illuminating London's bridges for the world’s longest public art commission
Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.
A small city lighting the way with connected street lighting – Ribeira, Spain
Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.
Solar Streelighting at Falcon City of Wonders, Dubai
Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.
Sheffield Tramline
Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps
Municipalities of Veneto
Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.
Public lighting renewal in Roztoky
Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.
Creating a vibrant city center – Smart Lighting
The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.
Ningbo, China enhances its skyline with connected LED lighting
Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.
Starting a project?
We’d love to hear from you.