A brighter future for the Port of Bilbao
A brighter future for the Port of Bilbao

A brighter future for the Port of Bilbao

Port of Bilbao Spain

The Port of Bilbao is one of the most important transport and logistics centers in the European Atlantic Arc. The port is an important entry point for cargo and cruise ships, and provides a railway connection to its dry dock network.

Customer challenge

To maintain its important role and establish itself as an innovator among ports, the Port of Bilbao embarked on an extensive renovation project. One of the key goals for the project was to modernize the existing lighting in order to reduce energy costs and make lighting management easier. Additionally, the port wanted to improve visibility and create lighting uniformity to increase the feeling of safety for workers and visitors.

Solution

Impressed by the lighting installation they had seen at the Ports of Tenerife, the Port Authority of Bilbao was confident about the benefits of connected LED lighting controlled and managed by Interact City software. The lighting installation at the Port of Bilbao includes more than 1,000 Philips ClearFlood LED floodlights, 540W and 270W LED floodlight with 60 degrees of asymmetry, to avoid light pollution, all connected to Interact City Lighting asset management software. The software enables single and group control of all connected light points, which can be managed and controlled remotely using a single intuitive dashboard. Interact City Lighting asset management software allows the Port Authority to control and manage lighting at the port, as well as on the railway platform and the dry dock.

Discover other case studies

Federation Square by bluebottle

bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.

A sustainably designed city – Gaiserwald, Switzerland

IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.

Joint vision brings smart lighting to citizens – Rogaland, Norway

Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.

Smart Street Lighting NY and Interact

NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.

Illuminating London's bridges for the world’s longest public art commission

Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.

A small city lighting the way with connected street lighting – Ribeira, Spain

Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.

Solar Streelighting at Falcon City of Wonders, Dubai

Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.

Sheffield Tramline

Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps

Municipalities of Veneto

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Public lighting renewal in Roztoky

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Creating a vibrant city center – Smart Lighting

The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.

Ningbo, China enhances its skyline with connected LED lighting

Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.

Starting a project?

Starting a project?

We’d love to hear from you.