A safer and more sustainable port
A safer and more sustainable port

A safer and more sustainable port

The Port of Antwerp

Belgium

Interact City was installed at The Port of Antwerp to help site managers achieve their sustainability goals while enhancing operational efficiency.

“Our focus is on strategic objectives such as safety and security, operational excellence, sustainable growth, mobility and transition. Interact City and LED lighting help us in achieving these goals.”

- Peter Melis, Senior Technical Project Manager, Port of Antwerp

Customer challenge

As the continent’s second largest port, the Port of Antwerp plays an important role in the European economy. All eyes will be on it in the coming years as it focuses on sustainability, safety and digitalization. With the help of Interact City, the Port of Antwerp wanted to become the first port in the Benelux with a connected lighting system.

Interact City contributes to a sustainable future

 

The operation began in 2018. Old gas discharge lamps made way for an energy-saving Interact City system comprising 1,300 Digistreet connected LED luminaires. The network was completed in mid-2019, and configured in close consultation with the Port of Antwerp. By employing open APIs, Interact City is now fully integrated with the port’s existing monitoring system.

 

The combination of connected LED lighting and Interact City software delivers considerable savings on energy costs. The Port of Antwerp has equipped its luminaires with a double set of connectors. By connecting plug-ins, environmental conditions — such as motion, traffic and noise — can be measured anywhere. Interact City turns the lighting network into the backbone of the port’s smart infrastructure. This helps to create a smart, sustainable port area that is in line with stakeholders’ wishes for achieving operational excellence.

 

The Port of Antwerp also wants to maintain an energy efficient working environment for its users in accordance with ISO 50001, and Interact City helps to meet this goal. Luminaire performance can be tracked online by port management. Faults are prevented or detected rapidly, so that action can be taken immediately. The Port of Antwerp also opted for LED to ensure safe traffic signals. Under gas discharge lighting, signaling colors such as red, orange or green can appear different, whereas they retain their true color with LED lighting. In addition, various dimming profiles ensure that the lighting in each port area is on at the right time, with the right lumen intensity.

Discover other case studies

Federation Square by bluebottle

bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.

A sustainably designed city – Gaiserwald, Switzerland

IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.

Joint vision brings smart lighting to citizens – Rogaland, Norway

Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.

Smart Street Lighting NY and Interact

NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.

Illuminating London's bridges for the world’s longest public art commission

Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.

A small city lighting the way with connected street lighting – Ribeira, Spain

Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.

Solar Streelighting at Falcon City of Wonders, Dubai

Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.

Sheffield Tramline

Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps

Municipalities of Veneto

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Public lighting renewal in Roztoky

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Creating a vibrant city center – Smart Lighting

The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.

Ningbo, China enhances its skyline with connected LED lighting

Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.

Starting a project?

Starting a project?

We’d love to hear from you.