Hillwood Polska fights light pollution with Signify
Hillwood Polska fights light pollution with Signify

Hillwood Polska fights light pollution with Signify

Hillwood, Poland

Poland’s leading commercial real estate developer turns to connected light.

"Hillwood's goal has always been to create modern warehouse facilities while also taking care of the neighborhood and the natural environment.”


Renata Michalczyk Head of Asset & Property Management, Hillwood Polska

The Challenge

Outdoor lighting on warehouse buildings can lead to light pollution, negatively affecting the nearby environment. Aiming to act responsibly, Hillwood has implemented steps to limit this issue. At its Janki Sokołów logistics center, Hillwood chose a lighting system from Signify that focuses illumination precisely where and when it’s required, helping to minimize the impact on the surroundings.

 

“At Hillwood, we prioritize environmental and nature conservation,” explains Emilia Bigos, Property Manager at Hillwood Polska. “We’re also mindful of the local community, which is why we’ve taken steps to reduce light pollution near our sites. We sought a solution that would lessen environmental and community impact while offering flexibility in lighting control and cutting down on energy use. That led us to partner with Signify.”

The Solution

 

Hillwood replaced the old LED lighting fixtures on the building exteriors with high-efficiency Philips UniStreet gen2 LED luminaires from Signify. Although these luminaires are typically used as cobra heads for roadway lighting, Hillwood made the unusual decision to mount them directly on the building façades. The angle of the luminaires and the light distribution were controlled so that only the Hillwood building itself is illuminated, leaving the surrounding areas dark. The UniStreet luminaires were integrated with an Interact connected LED lighting management system from Signify, specifically designed for city lighting. With Interact’s scene management capabilities, Hillwood can schedule the luminaires to dim to 25% at night, when only safety and security activities are taking place. This not only minimizes light pollution around the building, but it also saves the company energy.

 

Integrating the luminaires with Interact brings additional benefits in terms of increased flexibility and control. The system allows for flexible grouping of luminaires, smooth dimming, defining different lighting behaviors for different areas of the facility, and simplifying and improving lighting maintenance.

Discover other case studies

Federation Square by bluebottle

bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.

A sustainably designed city – Gaiserwald, Switzerland

IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.

Joint vision brings smart lighting to citizens – Rogaland, Norway

Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.

Smart Street Lighting NY and Interact

NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.

Illuminating London's bridges for the world’s longest public art commission

Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.

A small city lighting the way with connected street lighting – Ribeira, Spain

Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.

Solar Streelighting at Falcon City of Wonders, Dubai

Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.

Sheffield Tramline

Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps

Municipalities of Veneto

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Public lighting renewal in Roztoky

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Creating a vibrant city center – Smart Lighting

The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.

Ningbo, China enhances its skyline with connected LED lighting

Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.

Starting a project?

Starting a project?

We’d love to hear from you.