Greater efficiency and reduced costs with Interact City
Greater efficiency and reduced costs with Interact City

Greater efficiency and reduced costs with Interact City

Knittelfeld

Austria

As part of Knittelfeld’s commitment to urban development, the municipality undertook a project involving the upgrade of 2,000 light points to LED, controlled remotely via Interact City software.

“Our lighting is so innovative and efficient that we’ve managed to save 20% on total cost of ownership and cut energy costs by 80%.”

- Gerald Schmid, Mayor of Knittelfeld

Customer challenge

Before renewing its street lighting system, Knittelfeld set out three primary objectives: improve road safety, save energy and simplify the day-to-day management of lighting operations. The municipality needed a public lighting system capable of measuring, managing and monitoring all connected street lighting from a virtual map-based view in close to real-time. In addition, the system needed to run securely and remotely on a standard web browser via their existing network.

Simplified management of all connected light points

 

As part of this ambitious project, 2,000 inefficient high-pressure mercury-vapor luminaires were replaced with energy-saving LEDs and connected to the city's IT system via the Interact City software management system.

 

Interact City Lighting asset management software enables the new luminaires to automatically locate and commission themselves, as well as transmit data about their status. As soon as the LED luminaires are integrated with the software, people like Harald Bergman, Knittelfeld’s Head of Public Lighting, can track the luminaires’ performance and adjust street lighting levels almost instantly via a centralized dashboard.

 

The intuitive interface makes performing management tasks easy and convenient. In addition, automatic fault detection lets system users know where an outage has occurred so that maintenance crews can be dispatched quickly.

 

The connected luminaires relay performance data, including lighting levels and energy consumption. This data can be used to gain insights into the city’s lighting infrastructure. Maintenance and fault reports can be generated to provide a historical view of lighting performance, allowing the city to adjust the lighting as needed, and plan maintenance tasks to avoid downtime.

 

User-friendly Interact City Scene management software enables each luminaire to be managed individually or in groups to perform close to real-time or prescheduled actions.

Discover other case studies

Federation Square by bluebottle

bluebottle expanded Fed Square’s iconic façade lighting, delivering a new architectural system that illuminates the rear of the building, The Ian Potter Centre: NGV, and the car park façade. Dynamic strip and spot lighting now extend Fed Square’s night-time identity with a cohesive, event-responsive glow.

A sustainably designed city – Gaiserwald, Switzerland

IBG engineering spearheaded Gaiserwald’s sustainable and energy-efficient connected LED lighting transformation, managed and controlled by Interact City.

Joint vision brings smart lighting to citizens – Rogaland, Norway

Eleven towns in Rogaland, Norway have been transformed by installing 18,000 connected light points, managed and controlled remotely via Interact City.

Smart Street Lighting NY and Interact

NYPA will replace 500K street lights in NY state with connected LEDs by 2025. Interact City transforms these systems into a platform for smart city deployments.

Illuminating London's bridges for the world’s longest public art commission

Featuring artwork by world-renowned lighting artist Leo Villareal, the Illuminated River Project will become the longest public art installation in the world once complete.

A small city lighting the way with connected street lighting – Ribeira, Spain

Ribeira upgraded 8,600 street and urban light points to LED luminaires, over 6,500 of which are managed and controlled via Interact City.

Solar Streelighting at Falcon City of Wonders, Dubai

Signify ‘s vertically integrated solar street lighting helps falcon city of wonders to significantly contribute towards the project sustainability goals.

Sheffield Tramline

Sheffield Stagecoach upgraded the lighting for all platforms on the Sheffield Supertram, using Philips TrueForce Core LED Road Lamps

Municipalities of Veneto

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Public lighting renewal in Roztoky

Signify provided Philips SunStay solar or hybrid-powered luminaires, improving the lighting in eight different municipalities across the Veneto region in Italy.

Creating a vibrant city center – Smart Lighting

The city of Veghel needed a smart lighting solution that would bring back commerce and make the town a more desireable leisure destination.

Ningbo, China enhances its skyline with connected LED lighting

Ningbo, a city in eastern China, is boosting tourism and driving economic growth with dynamic architectural lighting controlled by Interact Landmark.

Starting a project?

Starting a project?

We’d love to hear from you.