Advanced Philips LED grow lights give you precise control over plant growth, enabling higher yields, consistent crop quality, and year-round production.
LED grow lights for tomatoes, other vegetables and fruits
Philips LED grow lights support consistent crop quality and yield without adding extra heat. Grow lights for tomatoes, other vegetables and fruits can supplement natural light with the spectrum and intensity crops need, all year round. They can be used for high-wire vegetables, leafy vegetables, herbs and soft fruits grown in greenhouses or indoor facilities, while reducing electricity use compared with HPS lighting.
No matter where you are in your lighting journey, we’re here to help you take the next step. Select the situation that best matches your greenhouse and discover the solutions, insights, and expertise tailored to your needs.
Philips GreenPower LED toplighting force elite
Optimized performance with intelligent control
Philips GreenPower LED toplighting force performance
Reliable LED performance and smart investment
Philips GrowWise control
Manage recipes and control every site, from anywhere
Philips GrowWise smart spectrum
Automatically optimize spectrum and manage energy spend
Philips GreenPower LED toplighting compact
The easy, flexible switch to LED
Philips GreenPower LED toplighting linear
Uniform light for flexible installations
Philips GreenPower LED interlighting
Targeted canopy light where you need it the most
Philips GreenPower LED flowering lamp
Extend daylight to boost crop results
High-performance fixtures, controls and apps work together to optimize lighting throughout the crop cycle. By responding to growing conditions, energy prices and production needs, the integrated system helps growers achieve higher and more consistent yields, maintain crop quality, reduce energy costs and make their operation more predictable.
Lights
Philips grow lights put you in full control of light intensity, spectrum, and power usage. With steerable channels, you can precisely tailor lighting to meet the unique needs of your crops and your business.
Controls
Easily create and manage custom light recipes for each crop phase or variety. GrowWise control simplifies recipe management and integrates seamlessly with your climate computer.
Apps
Smart apps automatically optimize your lighting system based on real-time factors like growing conditions, energy prices, and market demand – to increase yields or reduce energy costs.
Two growers optimize energy and crop performance
Botany Group saves energy, while Wim Peters Kwekerijen achieves around 2% more light on the crop without exceeding its planned power budget.
Den Berk Délice grows high-quality tomatoes with dimmable LED
See how precise light and climate control accelerate growth, improve crop quality and support predictable, energy-efficient production.
Great Lakes optimizes cucumber production with dimmable LED
Discover how flexible light levels and GrowWise control support healthy crops, consistent quality and efficient year-round production.
Genson improves strawberry quality with intelligent LED lighting
Learn how tailored light recipes and automatic dimming improve strawberry quality, worker comfort and energy efficiency in winter.
Equinox delivers uniform leafy greens with Philips LED
See how uniform, high-output LED lighting supports predictable yields, crop quality and efficient year-round leafy green production.
Truly Green Farms produces tomatoes through the winter
Discover how precise LED light control enables reliable winter tomato production without excess heat and supports year-round supply.
Bustanica grows over 1 million kg of leafy greens a year
See how tailored Philips LED light recipes enable reliable, resource-efficient leafy green production in Dubai’s desert climate.
One Farm increases annual growth cycles from 11 to 15
See how Philips LED lighting shortened winter cultivation from 88 to 62 days, increasing yields and stabilizing year-round supply.
VAXA grows 1 million lettuce heads a year in Iceland
Discover how Philips LED supports pesticide-free local production with ten times the output of a greenhouse and consistent year-round quality.
Practical insights for smarter growing
Frequently asked questions
Find answers about using Philips LED grow lights for vegetables & fruits to improve yield, crop quality and year-round production.
Toplighting fixtures sit above the crop and deliver the main production light. Philips GreenPower LED interlighting is installed within the canopy itself, placing targeted light where the crop needs it most - valuable for high-wire crops such as tomatoes and cucumbers, where light from above reaches the lower canopy poorly or when there is an abundance of sunlight. Many growers combine both for optimal crop performance.
Yes. Because LED lighting produces less radiant heat than HPS, you will need to adjust your greenhouse climate settings. A holistic strategy should also account for dehumidification. The advantage is that light and temperature can be controlled independently, giving you greater flexibility to balance crop needs, energy use and climate.
Philips GrowWise control lets you build and manage light recipes for each crop phase or variety, and integrates with your climate computer. Smart apps then respond automatically to growing conditions, energy prices and production needs. Wim Peters Kwekerijen achieved around 2% more light on the crop without exceeding its planned power budget, while Botany Group aimed the same system at saving energy.
Philips LED grow lights supplement changing levels of natural daylight with controlled light intensity and spectrum. This helps maintain more stable growing conditions across seasons, supporting consistent crop quality, yield and production planning. The right light recipe depends on the crop, growth phase, greenhouse conditions and your production targets.
Start with the crop, cultivation system and production goals. A lighting plan should account for required light levels, spectrum, uniformity, growing area, installation height and the role of daylight. It should also align with heating, humidity and energy strategies. Signify and its certified partners can help develop an integrated solution for your facility.