What would “future-ready” lighting actually look like?
Future-ready lighting simplifies what is currently complex. Instead of manually adjusting settings and trying to predict outcomes, your lighting system supports you in making the right decision—based on real-time conditions and prediction models. It takes into account factors like sunlight, crop stage, and operational priorities, and translates these into optimized lighting automatically. You don’t need to manage every parameter. You define your goal—whether that’s saving energy or maximizing light output—and the system adapts accordingly. At the same time, you remain in control. You have clear insights into what is happening and why, without needing to search for information across different tools and platforms. In that sense, future-ready lighting is not about adding more functionality. It’s about making advanced capabilities accessible, transparent, and easy to use in your daily operation.
How can I steer my lighting without risking my crop or business results?
This is where many growers hesitate today. You know that adjusting spectrum can unlock additional value. But you also know that it can affect both your power budget and your light output. And once those start to shift unexpectedly, your carefully planned strategy becomes harder to control. This is exactly the challenge that the next generation of lighting apps is designed to solve. GrowWise smart spectrum automatically applies knowledge on plant-light interaction built on 20 years of research, to adjust your lighting within controlled boundaries. In practice, this means you can optimize your spectrum without deviating from your planned power budget or your desired light output. You can define minimum light levels per color for specific time periods, including sunrise and sunset dependencies, so smart spectrum can optimize within grower-defined constraints. This makes it possible to safeguard settings such as minimum blue and green levels for bumble bee light, directly within the GrowWise control environment when setting up a recipe. The system continuously balances the variables for you, ensuring that adjustments remain safe and predictable. Instead of avoiding changes, you can start using them—with confidence.
How can GrowWise smart spectrum improve my business performance?
Once spectrum steering becomes easier to manage and more reliable, it starts to contribute more directly to your business performance. Small improvements—slightly lower energy use or slightly higher light output up to 7%—add up over time with a yield increase as a result. They influence your energy costs, your production levels, and ultimately your margin. At the same time, the operational side becomes simpler. You spend less time adjusting settings, less time analysing trade-offs, and less time chasing optimal results manually. An interactive long-term dashboard also gives you insight into lighting performance across multiple growing periods, helping you analyse results over time and continuously improve your lighting strategy. As confirmed by Wilbert van Bussel, Operations Manager, Wim Peters Kwekerijen: You gain in crop growth and development while hardly having to do anything extra yourself. You set the parameters once, and the system does the rest. The algorithm delivers real quick wins.”
Lighting shifts from being a technical task to being a strategic lever. It helps you respond not only to plant needs, but also to external factors such as energy pricing or market demand. And perhaps most importantly, it gives you predictability—allowing you to make decisions with greater confidence. Van Bussel agrees: “We saw a slightly stronger crop and heads in the section where we used the smart spectrum app. The biggest gains are at the edges of the lighting season, when there is more natural daylight and you can benefit from switching the lighting quickly.