Sparta Boxing Club Transformed with NatureConnect
Sparta Boxing Club Transformed with NatureConnect

Sparta Boxing Club Transformed with NatureConnect

Sparta Boxing Club, Bergen, Norway

Bergen Sparta Boxing Club in Bergen installed the NatureConnect by Signify, designed to replicate natural daylight. The boxing club is located in an old bomb shelter, built into a mountain with no natural daylight. With NatureConnect, they have succeeded in creating a truly unique lighting experience that enhances the atmosphere and improves light performance.

“The light has really transformed the space and made it an even better place for our members. It has been a pleasure working with Signify and LOS Elektro on this project. We look forward to continuing to upgrade the lighting in the club with their help."

Bjarte Ness, representative of Sparta Boxing Club

Customer Challenge

Natural daylight is a luxury when you're in a room without windows, and the members of Bergen Sparta Boxing Club know this all too well. However, they've now invited the light in with NatureConnect by Signify, which provided a custom solution for the club's multifunctional training room. The NatureConnect system was installed by the Norwegian company LOS Elektro and completed in September 2024. Since then, the club’s members have been very satisfied with the new lighting, which has created an entirely new atmosphere in what was previously a dark training space.

Solution

NatureConnect is designed to mimic the natural rhythm of daylight, creating a sense of well-being and energy in the space. The settings can easily be adjusted via wall-mounted switch panels to suit different activities, making it ideal for the multifunctional training room that Bergen Sparta Boxing Club uses for everything from boxing training to table tennis and community events.

 

For more information:

 

www.signify.com/NatureConnect

Discover other case studies

Vienna City Hall: dynamic, energy‑saving lighting upgrade

Discover how Vienna City Hall gained dynamic color-changing lighting, improved efficiency, and preserved its historic character with Color Kinetics luminaires.

Central Criminal Courts of Justice by Eclipse Integration

Faced with an aging and failing Light Master system and an emergency lighting installation that no longer met compliance standards, the building operators required an upgrade strategy that would restore full regulatory compliance and operational reliability—while ensuring the building remained fully functional with zero downtime throughout the installation process.

Australian War Memorial by bluebottle

bluebottle continues its work on one of Australia’s most significant cultural redevelopments: the Australian War Memorial. The team delivered an integrated lighting-control solution through Dynalite, enabling smooth transitions, intuitive scene recall and reliable connection to the broader building systems—supporting a project of true national importance.

Connected bridge lighting – San Francisco Bay Bridge

The LED lighting sculpture with remote monitoring over Interact Landmark software had such a broad social and economic impact on the Bay Area that the temporary display became a permanent part of the skyline.

Ministry of foreign and European affairs by Lipapromet

Earthquake damaged building. Complete renovation of the building including new exterior decorative lighting. Using Philips Uni portfolio with DMX communication protocol and Dynalite lighting control system

Dynamic LED lighting – remote controls

CEPSA was interested in saving costs and improving operational efficiency with an LED lighting system that could be easily controlled and managed from a single dashboard using connected lighting management software.

GEM: Lighting Egypt's History Near the Pyramids of Giza

GEM, near the Pyramids of Giza, features a cutting-edge lighting system to showcase Egypt's ancient artefacts, boosting tourism with over 5M visitors annually.

De Zwerm Underpass, Eindhoven, the Netherlands

Eindhoven’s De Zwerm underpass lighting display is the perfect combination of art and functional, connected lighting.

Smart bridge lighting - Big River Crossing

The Harahan Bridge and adjacent Big River Crossing boardwalk illuminate the sky with new dynamic LED lighting powered by Interact Landmark software.

Citizen House Odense

The lively Citizen house of Odense has become an attractive meeting point thanks to a gold finish and the use of light, including Color Kinetics lighting.

Jumeirah Emirates Towers

Jumeirah Emirates Towers shines with smart LED lighting, saving energy while preserving elegance and supporting Dubai’s green vision.

Starting a project?

Starting a project?

We’d love to hear from you.