The stunning De Zwerm Underpass lighting display has become a major new landmark in Eindhoven.
De Zwerm Underpass
Eindhoven, the Netherlands
“The continuously responsive movements of De Zwerm make it not just another static work of art in the city but a truly living organism integrated in the urban landscape.”
- Frank Tjepkema, Designer of De Zwerm Underpass
Customer challenge
Also known as “The City of Lights,” Eindhoven has had a relationship with lighting and technology that goes back a long time. However, some areas lack the character that the city is famous for. The Eindhoven municipality wanted a living, breathing artwork piece which reflected the city’s past, strengthened the identity of an anonymous part of town, and acted as a visual connection between traffic flows above and below the tunnel.
Photo Credits: © Frank Tjepkema, Studio Tjep
A landmark like no other
Inspired by a flock of birds, Frank Tjepkema — the lighting designer responsible for De Zwerm — combined 728 steel elements and 1,456 individually controlled LED nodes to create a unique lighting display that has become an instant landmark in Eindhoven.
De Zwerm, which means “the swarm,” features a sophisticated interplay between direct and indirect lighting: carefully positioned light from inside each “bird” shines into the next one in a way that optimizes reflection in a smooth transitional movement. This creates an area of light rather than a spotlight, never shining directly into the eyes of drivers.
The optical illusion of the flock of birds is a great example of how lighting and technology can combine impressively.
Each “bird” is outfitted with two Color Kinetics iColor Flex LMX gen2 LED nodes that instantly change color and brightness. The dynamic lighting display changes depending on temperature and traffic flow. In warmer seasons, drivers see reds and oranges while colder weather brings blues and greens. Interact Landmark connected lighting software enables easy monitoring, management and control of the installation. It works seamlessly with Color Kinetics fixtures and the Philips BaseLogic lighting system.
Inside the tunnel, the focus is more on driver comfort and safety. The underpass interior is equipped with Philips BaseLogic system. A photometer on the outside of the underpass records light levels and adjusts the output of the luminaires inside to ensure drivers can see in front of them safely and comfortably.
Discover other case studies
Vienna City Hall: dynamic, energy‑saving lighting upgrade
Discover how Vienna City Hall gained dynamic color-changing lighting, improved efficiency, and preserved its historic character with Color Kinetics luminaires.
Central Criminal Courts of Justice by Eclipse Integration
Faced with an aging and failing Light Master system and an emergency lighting installation that no longer met compliance standards, the building operators required an upgrade strategy that would restore full regulatory compliance and operational reliability—while ensuring the building remained fully functional with zero downtime throughout the installation process.
Australian War Memorial by bluebottle
bluebottle continues its work on one of Australia’s most significant cultural redevelopments: the Australian War Memorial. The team delivered an integrated lighting-control solution through Dynalite, enabling smooth transitions, intuitive scene recall and reliable connection to the broader building systems—supporting a project of true national importance.
Connected bridge lighting – San Francisco Bay Bridge
The LED lighting sculpture with remote monitoring over Interact Landmark software had such a broad social and economic impact on the Bay Area that the temporary display became a permanent part of the skyline.
Ministry of foreign and European affairs by Lipapromet
Earthquake damaged building. Complete renovation of the building including new exterior decorative lighting. Using Philips Uni portfolio with DMX communication protocol and Dynalite lighting control system
Dynamic LED lighting – remote controls
CEPSA was interested in saving costs and improving operational efficiency with an LED lighting system that could be easily controlled and managed from a single dashboard using connected lighting management software.
GEM: Lighting Egypt's History Near the Pyramids of Giza
GEM, near the Pyramids of Giza, features a cutting-edge lighting system to showcase Egypt's ancient artefacts, boosting tourism with over 5M visitors annually.
Smart bridge lighting - Big River Crossing
The Harahan Bridge and adjacent Big River Crossing boardwalk illuminate the sky with new dynamic LED lighting powered by Interact Landmark software.
Citizen House Odense
The lively Citizen house of Odense has become an attractive meeting point thanks to a gold finish and the use of light, including Color Kinetics lighting.
Jumeirah Emirates Towers
Jumeirah Emirates Towers shines with smart LED lighting, saving energy while preserving elegance and supporting Dubai’s green vision.
Starting a project?
We’d love to hear from you.