Central Criminal Courts of Justice

Central Criminal Courts of Justice

By Eclipse Integration

Central Criminal Courts of Justice

Central Criminal Courts of Justice

Dublin, Ireland

Faced with an aging and failing Light Master system and an emergency lighting installation that no longer met compliance standards, the building operators required an upgrade strategy that would restore full regulatory compliance and operational reliability—while ensuring the building remained fully functional with zero downtime throughout the installation process.

Challenge

Customer challenge

As Ireland’s Central Criminal Courts, the client required a solution that not only met strict compliance and energy-efficiency requirements but, above all, ensured absolutely no disruption to the building’s operation or security. To identify the most appropriate approach, the building operators went to market and reviewed a range of proposals—spanning wireless, wired, and several hybrid solutions—each offering different pathways to achieving the required upgrade.

Solution

The solution

Eclipse Integration selected the Dynalite system as the ideal solution to deliver the required controls upgrade. When combined with our ABB DALI emergency lighting system, it provided the perfect balance of compliance, reliability, and energy management. Eclipse delivered the full turnkey package—including design, installation, commissioning, and certification—ensuring a seamless experience for the client.

Our modular project-delivery approach guaranteed zero downtime, a key requirement for the Central Criminal Courts. Through extensive offsite build and pre-commissioning, our installation teams were able to work overnight, returning the courts to full operational readiness every morning.

Over the course of 10 months, Eclipse successfully installed and commissioned:

  • 1,600 control devices
  • 2,900 emergency lighting units
  • 3,000+ pre-fabricated leads

The completed system provides a fully graphical interface for real-time testing and monitoring of the new emergency lighting installation. In addition, this phase of works has prepared the building’s infrastructure for the next stage of the upgrade—set to introduce more than 6,200 DALI lighting points across the site.

Team

Certified System Integrator: Eclipse Integration

Lighting Designer: Eclipse Integration

Client / end user: Group 4 Security

Contractor: Lean Electrical Engineering 

Products

Dynalite: DBC905, DUS360CR, PDDEGs, DDBC320, System Manager

Discover other case studies

Vienna City Hall: dynamic, energy‑saving lighting upgrade

Discover how Vienna City Hall gained dynamic color-changing lighting, improved efficiency, and preserved its historic character with Color Kinetics luminaires.

Australian War Memorial by bluebottle

bluebottle continues its work on one of Australia’s most significant cultural redevelopments: the Australian War Memorial. The team delivered an integrated lighting-control solution through Dynalite, enabling smooth transitions, intuitive scene recall and reliable connection to the broader building systems—supporting a project of true national importance.

Connected bridge lighting – San Francisco Bay Bridge

The LED lighting sculpture with remote monitoring over Interact Landmark software had such a broad social and economic impact on the Bay Area that the temporary display became a permanent part of the skyline.

Ministry of foreign and European affairs by Lipapromet

Earthquake damaged building. Complete renovation of the building including new exterior decorative lighting. Using Philips Uni portfolio with DMX communication protocol and Dynalite lighting control system

Dynamic LED lighting – remote controls

CEPSA was interested in saving costs and improving operational efficiency with an LED lighting system that could be easily controlled and managed from a single dashboard using connected lighting management software.

GEM: Lighting Egypt's History Near the Pyramids of Giza

GEM, near the Pyramids of Giza, features a cutting-edge lighting system to showcase Egypt's ancient artefacts, boosting tourism with over 5M visitors annually.

De Zwerm Underpass, Eindhoven, the Netherlands

Eindhoven’s De Zwerm underpass lighting display is the perfect combination of art and functional, connected lighting.

Smart bridge lighting - Big River Crossing

The Harahan Bridge and adjacent Big River Crossing boardwalk illuminate the sky with new dynamic LED lighting powered by Interact Landmark software.

Citizen House Odense

The lively Citizen house of Odense has become an attractive meeting point thanks to a gold finish and the use of light, including Color Kinetics lighting.

Jumeirah Emirates Towers

Jumeirah Emirates Towers shines with smart LED lighting, saving energy while preserving elegance and supporting Dubai’s green vision.

Starting a project?

Starting a project?

We’d love to hear from you.