See shopping in a new light with "Find my product" app
See shopping in a new light with "Find my product" app

See shopping in a new light with "Find my product" app

Albert Heijn

Hoofddorp, the Netherlands

With Indoor navigation integrated in the ‘Find my product’ app, Albert Heijn Hoofddorp, can now efficiently help shoppers to find everything they need, enhancing the shopping experience and avoiding lost sales.

“This technology truly offers infinite possibilities.”

- Steven de Kroes, Format developer Albert Heijn

Customer Challenge

Albert Heijn is committed to making grocery shopping and cooking easier for customers. This can be a challenge if customers can’t find all the products on their list. Independent research* conducted with 1,000 Dutch shoppers found that 14% occasionally cannot find products when shopping. This relates to many different products, not just a few items they only occasionally buy or are poorly-placed. And although 75% of those shoppers would eventually try to find those products themselves, 44% would still leave store having bought at least one product fewer than planned for. What Albert Heijn needed was a solution that would help shoppers to find every product quickly and easily

 

 

 

*CG Research commissioned by Signify. October 2018

Solution

Our solution connects the Interact Retail Indoor navigation system to Albert Heijn’s product data base in one app, making it possible to locate every item that is sold in the store with a hyper-accuracy of 30 cm/1 ft.

 

Each light point in the store sends a unique code that is captured by the front camera of a smart device, providing the location of the shopper and combining that with the location of the product. Customers can then follow a dynamic route on a digital map that takes them to the product using the shortest route to the shelf.

 

The system also provides retailers with location analytics such as dwell time, footfall and density helping them to improve business and marketing initiatives.

Interact – shopping made simple

The “Find my product” app harnesses the power of connected lighting in the store by using the Interact Retail navigation system to create a dynamic locations system. Qualitative research* shows the app is highly appreciated with a high usage intention. The most important benefits mentioned by users are the convenience of being able to find a product, the speed of finding a product versus searching or asking, and being independent from others to find it. Shoppers really appreciate the app, 84% gave it a "thumbs up."

 

*Research by PAM research & advice, commissioned by Signify, October 2018

Discover other case studies

Smart supermarket lighting – Globus

Globus supermarket was able to improve stopping power, increase dwell time and grow sales with soft pastel up-lights enabled by Interact Retail Scene management software.

Carrefour Circular Lighting

Carrefour is committed to sustainability, circularity and an enhanced shopping experience. With energy-efficient and circular lighting from Signify, CO₂ emissions are reduced whilst also creating a welcoming atmosphere for customers.

Chatswood Chase

The $625m Chatswood Chase redevelopment required a lighting control system as sophisticated as its incoming luxury retailers. A comprehensive Dynalite solution was deployed, seamlessly managing 2,656 lights to create a stunning retail journey. Dynalite with Enttec delivers dynamic 'wow' factors at the entries, while granular control and BMS integration ensure premium efficiency and experience throughout the centre.

Smart retail lighting reduces costs and improves customer experience

Interact Retail creates an enhanced in-store experience while reducing maintenance, installation and energy costs.

Smart supermarket lighting – Albert Heijn XL Eindhoven

See how Albert Heijn has reduced energy costs with smart lighting enabled by Interact Retail software, while delivering a superior, engaging in-store experience for customers.

Castorama - A bright future for shopping within reach

Need help finding that one product in a store which offers over 35.000? Castorama, as the first DIY retailer in the world, responded to this challenge by introducing Interact Retail Indoor navigation.

An enhanced shopping experience – EDEKA Hamburg

EDEKA Hamburg has created an enhanced shopping experience by installing LED lighting controlled by Interact Retail software.

Location-based promotions – MediaMarkt, Eindhoven

MediaMarkt in Eindhoven creates a more intimate customer experience with its StoreGuide App and indoor positioning enabled by Interact Retail Indoor navigation software.

A smart lighting concept – E-Center Gaimersheim

The supermarket EDEKA is setting new standards with its smart lighting concept enabled by Interact Retail t at its flagship store in Gaimersheim.

Dior Gold House

Dior Gold House in Bangkok is a landmark retail destination where luxury scenography meets intelligent lighting control. A fully connected Dynalite system with automated DALI façade and interior control gives Dior flexible scenes for events, precise presentation lighting and a seamless visitor experience from garden arrival to boutique and Café Dior.

EDEKA Germany

EDEKA Clausen, from Germany, choses Philips UV-C air disinfection lighting to protect their stores against bacteria and viruses.

Starting a project?

Starting a project?

We’d love to hear from you.