A mostly empty office space with white walls, tiled flooring, ceiling panels, and a stepladder near a lone desk in the background

Codes and emergency lighting system planning

Codes and standards

Emergency lighting is a vital part of a facility's life safety program. While it is essential to consult federal, state and local codes related to emergency lighting for your project, there are some general guidelines for code requirements.

 

Although state and local building codes vary, most are based upon:

The National Electrical Code®, NFPA 70®, Article 700;
The Life Safety Code®, NFPA 101®, Sections 7-8 through 7-10;
The Occupational Safety and Health Act (OSHA), which offers some general guidelines.

Key information

These codes provide complete information on emergency lighting requirements; however, a good introduction is found in NFPA 101, Section 7.9.2.1–7.9.2.1.3:
 

"Emergency illumination shall be provided for a minimum of 1½ hours in the event of failure of normal lighting. Emergency lighting facilities shall be arranged to provide initial illumination that is not less than an average of 1 ft-candle (10.8 lux) and, at any point, not less than 0.1 ft-candle (1.1 lux), measured along the path of egress at floor level. Illumination levels shall be permitted to decline to not less than an average of 0.6 ft-candle (6.5 lux) and, at any point, not less than 0.06 ft-candle (0.65 lux) at the end of 1½ hours. The maximum-to-minimum illumination shall not exceed a ratio 40 to 1."
 

It is important to remember that code requirements reflect minimum standards and, therefore, are generally considered only a starting point in designing emergency lighting systems. Additional emergency lighting, beyond minimums, is warranted in some facilities, depending upon facility use and other relevant factors. Hospitals and nursing homes, for example, are excellent candidates for additional emergency lighting. The same is true of manufacturing and production areas, which often present numerous potential safety hazards even under the best of conditions.

Summary of requirements

Emergency lighting is required throughout the path of egress and must operate for a minimum of 90 minutes. (See NFPA® 101® Life Safety Code®.)
Stairs, aisles, corridors, ramps, escalators and passageways leading to safety must be continuously illuminated for a minimum of 90 minutes. Illumination times for Bodine fluorescent emergency ballasts, emergency LED drivers and emergency lighting inverters meet or exceed the National Electrical Code®, Life Safety Code® and UL 90-minute requirements. For codes requiring longer illumination times, Bodine offers models with two- and four-hour runtimes.

 
Emergency lighting transfer must be automatic. 
Transfer of emergency lighting must be automatic (within 10 seconds) of loss of the normal lighting supply power. Bodine fluorescent emergency ballasts, emergency LED drivers and emergency lighting inverters provide instant backup lighting when the normal supply of power fails. 

 
Emergency lighting must provide an average of 1 footcandle initial illumination. 
Emergency lighting facilities must provide initial illumination that is no less than an average of 1 footcandle (10.8 lux) and a minimum at any point of 0.1 footcandle (1.1 lux) measured along the path of egress at floor level. A maximum-to-minimum illumination uniformity ratio of 40 to 1 shall not be exceeded to minimize dark-to-bright spots. Proper placement of Bodine products will help ensure code compliance with regard to footcandle illumination. 

 
Changes in direction must be clearly marked. 
Changes in direction or routes that are not immediately apparent must be clearly marked. Specifying Bodine products in addition to other unit equipment helps ensure an adequate level of safety results.

 

UL product testing & code compliance
Bodine fluorescent emergency ballasts, emergency LED drivers, emergency lighting inverters and other products are tested by Underwriters Laboratories in accordance with the UL standards. These standards vary by product type but is primarily UL 924, “Emergency Lighting and Power Equipment”. Products are either:

UL Listed certification mark

UL Listed

UL Listed products for factory or field installation. The majority of Bodine products, of all types, carry the UL Listing and are ideal for field installation in order to retrofit existing luminaires/systems into code-complaint emergency lighting.

UL Recognized Component mark

UL Recognized

UL Recognized products are suitable for factory installation only. Certain Bodine products are optimized for the OEM (original equipment manufacturer) and must be originally installed in the factory. However, replacing a UL Recognized product in the field, this is allowed so long as the installation follows the OEM’s original method.

Maintenance

Codes mandate, among other actions and standards, periodic monitoring of emergency lighting equipment once it is installed. Emergency operation must be tested monthly (30 seconds) and, for battery-powered sources, annually (90 minutes) in order to meet the NFPA's Life Safety Code (see Section 7.9). Moreover, the NFPA requires that written records of these tests and their accompanying visual inspections be kept as proof of maintenance (see the Life Safety Code, Section 7.9 and the National Electrical Code, Article 700). Because this emergency equipment is used only on an emergency basis, it is important that regular maintenance be performed. As with all capital investments, upkeep is vital and provides proof when liability questions arise. Common sense must be used in planning emergency lighting systems. The major objective of adequate and reliable emergency lighting is to help ensure occupants a safe, panic-free exit from a building in the event of a power failure.
 

This section contains a revision of portions of a 1977 article written for EC&M by former Bodine Company CEO David Crippen.

Planning and specifying

Emergency lighting is a vital part of a facility's life safety program. It is important to carefully consider the needs of your facility to achieve the best results. Codes and regulations, such as the NFPA® 101® Life Safety Code®, establish guidelines for emergency lighting equipment. However, there may be circumstances that call for more than minimum standards. Incorporating the right combination of elements into emergency lighting design helps provide a higher degree of safety. The best emergency lighting system is carefully planned for a specific building and its occupants. This section includes a summary of some of the significant factors involved in this planning process.

An empty hospital corridor with white walls, wooden handrails, and a polished reflective floor

Proximity, shape and size of exits

The configuration of walls adjoining the exit way, the amount of space devoted to exit passages and travel distance to exits should be considered when determining the number and placement of emergency lighting units. For example, it is important to place emergency lighting at an intersection of a corridor or hallway. If it is a large area, additional units may be needed to provide adequate light to see any objects blocking the exit path.

Healthcare workers in a hospital corridor, with a person pushing a gurney and staff attending to a patient in a wheelchair

Intended use of a building

Additional emergency lighting may be required depending on the types of people using a facility. Elementary school children and older adults may require more emergency lighting than apartment residents, college students or office workers. Retail situations where valuable merchandise is accessible or high-security facilities may also require extra illumination. Adequate lighting can be especially critical in hospital settings (e.g., operating and emergency rooms).

A modern office lounge with bold red walls, two red leather chairs on grey carpet, and a frosted glass partition

Ceiling, floor and wall characteristics

Emergency lighting levels are affected by the color and texture of surrounding areas. Light-colored ceilings, walls and floors with smooth surfaces require less emergency lighting because of their reflective characteristics than do darker ceilings, floors and walls with rough surfaces.

Three colleagues in a glass-walled meeting room, with a fourth person entering through the corridor

Occupancy and building knowledge

The number of people expected to occupy a building and their knowledge of its interior also influence the level of emergency illumination needed. Large numbers of people unfamiliar with exit paths require more emergency lighting than smaller numbers of people who know the surroundings. Consequently, auditoriums, convention halls and sports arenas often need higher levels of emergency illumination than office buildings and warehouses.

Placement of emergency equipment

Strategically placed emergency lighting units help occupants avoid potential obstructions near the path of egress. Although exit signs with directional indicators are required and are important to occupant safety, emergency LED drivers and fluorescent emergency ballasts in corridors, intersections and stairwells assist occupants in clearly identifying the exit route. To ensure that emergency lighting is continuous throughout the path of egress, use emergency LED drivers and fluorescent emergency ballasts in addition to other emergency lighting unit equipment. Providing evenly spaced emergency lighting enhances the safe, quick movement to exits and prevents excessively bright-to-dark spots along the path of egress. Depending on the facility, it may be better to specify a greater number of emergency LED drivers or emergency ballasts with lower light levels than to specify a lesser number of widely spaced emergency fixtures with higher lumen output.

We'd love to hear from you