Philips Smart Lighting launches Screen Sync and Fairy String Lights

10 September 2026

Philips Smart Lighting brings Screen Sync and Fairy String Lights to life

 

  • New Screen Sync with Strip Light captures the entire television display and synchronizes color in real time with any on-screen content
  • New RGBIC Fairy String Lights, available in 10-, 15- and 20-meter lengths, bring millions of colors, preset effects and music sync to indoor and outdoor spaces1

 

Eindhoven, the Netherlands: Signify (Euronext: LIGHT), the world leader in lighting, is expanding Philips Smart Lighting with two product launches designed to make connected lighting more immediate, expressive and easy to enjoy. The new Screen Sync with Strip Light turns television content into responsive, room-filling color, while the new RGBIC Fairy String Lights bring flexible ambience to celebrations and everyday moments indoors and outdoors1.
 

Immersion made easy - with any content on screen
 

Philips Smart Lighting Screen Sync with Strip Light brings movies, television and sport beyond the edges of the display. A fisheye lens captures the full screen from edge to edge, reading its colors in real time and reproducing them through a four-sided RGBIC strip light mounted behind the television.

 

Because the device responds directly to what appears on the screen, it can synchronize with native smart-TV apps, broadcast television, and HDMI-connected devices. Consumers will not have to route their entertainment through a separate HDMI source, making it easy to enjoy responsive lighting with content from any source. 

 

Installation is designed to be straightforward. Users position the Screen Sync device on top of the television and start calibration in the app. The device automatically aligns its anchor points with the screen, with the option to make manual adjustments afterwards.

 

Preset sync modes can tailor the effect to different viewing experiences, while a built-in microphone can make the lights respond to music. Consumers who want to extend the experience across the room can add compatible Philips Smart Lighting bulbs, lightstrips and lamps.

One complete kit, shaped around the television

 

Screen Sync with Strip Light is offered as a complete kit in versions designed for televisions from 40 to 50 inches, 55 to 65 inches and 75 to 85 inches. The strip delivers smooth multicolor gradients around all four sides of the screen, creating a continuous surround-lighting effect. Each kit includes both the Screen Sync device and Strip Light, so consumers do not need to select or purchase the components separately.

 

Decorative color, wherever the moment happens

 

The new Philips Smart Lighting RGBIC Fairy String Lights extend dynamic color throughout the home. Available in 10-, 15- and 20-meter lengths, they combine millions of colors with preset effects such as chasing rainbows, soft fades and sparkling accents. Their long, flexible format makes it easy to decorate bedrooms and living spaces, create a colorful backdrop for parties, or bring atmosphere to gardens and outdoor gatherings.

 

Powered through USB-C, the Fairy String Lights can also be connected to a power bank, giving consumers the freedom to place them without needing a nearby outlet. They can be controlled through the app, compatible accessories or voice commands. Music sync makes the lights pulse to the beat when a smartphone is kept near the sound source.

 

The lighting and controller are IP65-rated, making the Fairy String Lights suitable for indoor and outdoor use.1

Consumers want richer experiences at home, and they expect technology to be simple, flexible and accessible. Screen Sync brings movies, gaming and sport beyond the television using the content people already watch, without a complicated setup. Fairy Lights make it just as easy to create colorful ambience for everyday moments and celebrations, indoors or outdoors. Together, they show how Philips Smart Lighting makes expressive connected lighting easy to start, personalize and enjoy.”

 

Mafalda Monteiro,
Business leader Philips Smart Lighting

Availability

Availability varies by market. Local pricing and product availability should be confirmed through the relevant Philips Smart Lighting retail channels.

 

  • Philips Smart Lighting Screen Sync with Strip Light for 40-50-inch televisions - available in Europe and the UK, starting at EUR 89.99.
  • Philips Smart Lighting Screen Sync with Strip Light for 55-65-inch televisions - available in Europe, the UK and North America, starting at EUR 109.99 in Europe.
  • Philips Smart Lighting Screen Sync with Strip Light for 75-85-inch televisions - available in Europe and North America, starting at EUR 129.99 in Europe.
  • Philips Smart Lighting RGBIC Fairy String Lights, 10 m - available in Europe, starting at EUR 34.99.
  • Philips Smart Lighting RGBIC Fairy String Lights, 15 m - available in Europe, starting at EUR 49.99.
  • Philips Smart Lighting RGBIC Fairy String Lights, 20 m - available in Europe, starting at EUR 64.99.

 

Product videos 

https://youtu.be/WLglxSSNnLU 

About Philips Smart Lighting

 

Philips Smart Lighting brings simple and accessible connected lighting to everyday homes. Powered by the WiZ platform, Philips Smart Lighting products connect directly to your home Wi-Fi network and are controlled through the WiZ app. The range makes it easy to personalize lighting for different rooms, moods and moments. Philips Smart Lighting is a distinct connected lighting proposition from Philips Hue, with its own products, app and ecosystem.

 

Footnotes

[1]  The power supply unit is rated IP20 and must be placed indoors.

About Signify

 

Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers. We proudly bring to market the world’s best lighting brands, from Signify, Philips, Philips Hue, Signify Interact, Signify Dynalite, Color Kinetics and many more. Our advanced products connected systems and services unlock the extraordinary potential of light for brighter lives and a better world. In 2025, we had sales of EUR 5.8 billion, approximately 27,000 employees, and a presence in over 70 markets. We are in the Dow Jones Best-in-Class World Index earned a CDP ‘A’ score for climate performance and transparency and hold the EcoVadis Platinum rating.

 

News and updates from Signify can be found in the Newsroom, on LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

More press releases

  • Signify and Mercedes-AMG PETRONAS F1 Team extend partnership to drive performance and elevate experiences

    November 17, 2026

    Signify and Mercedes-AMG PETRONAS F1 Team extend partnership to drive performance and elevate experiences

  • Signify Interact upgrades Intelligent Systems

    November 10, 2026

    Signify Interact upgrades Intelligent Systems

  • Oxford analysis links circular approaches to business benefits in 74% of real-world lighting projects studied

    October 26, 2026

    Oxford analysis links circular approaches to business benefits in 74% of real-world lighting projects studied