Signify enables greater control and energy savings for site managers with Signify Interact motion and daylight DALI sensors
27 November 2025, Eindhoven, the Netherlands – Signify (Euronext: LIGHT) has launched a new mains-powered motion and daylight DALI (Digital Addressable Lighting Interface) sensor. The new sensor enables site managers to gain greater control over their lighting and save on energy costs by ensuring lights are only switched on when needed.
Designed to sit within the Signify Interact connected lighting platform, the DALI sensor can partner with a range of luminaire families including Maxos Fusion, GentleSpace and Pacific LED. Within this connected platform, users can access the sensor’s data metrics to fully optimise their lighting management.
The DALI sensor provides optimal coverage from ceiling heights ranging from 2 to 16 meters, making it ideal in industrial settings, such as manufacturing sites, warehouses, logistics centres, and indoor parking. Signify Interact’s suite of connected products in these environments provide high-quality lighting, asset management capabilities, and advanced lighting control, which can improve worker productivity, enhance safety, health and wellbeing, and bring energy, cost and time savings.
The sensor automatically adjusts lighting levels depending on the amount of daylight and uses Passive Infrared (PIR) motion detection technology to control luminaires. Featuring adjustable sensitivity, it can be used to adapt to specific environments and user behaviours. Its robust wireless Zigbee communication has a best-in-class range of 50 meters. Some variants of the sensor have high IP and IK ratings to withstand dust, water, and impact in tough environments.
The sensor supports the DALI 2 driver with parts 251, 252 and 253 for energy metrics and up to 10 DALI drivers can connect via an integrated DALI port of 20 mA. It can be commissioned using the Interact Pro app via Bluetooth and the IR remote control.
Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers. We proudly bring to market the world’s best lighting brands, from Signify, Philips, Philips Hue, Signify Interact, Signify Dynalite, Color Kinetics and many more. Our advanced products connected systems and services unlock the extraordinary potential of light for brighter lives and a better world. In 2025, we had sales of EUR 5.8 billion, approximately 27,000 employees, and a presence in over 70 markets. We are in the Dow Jones Best-in-Class World Index earned a CDP ‘A’ score for climate performance and transparency and hold the EcoVadis Platinum rating.
News and updates from Signify can be found in the Newsroom, on LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

October 26, 2026
Oxford analysis links circular approaches to business benefits in 74% of real-world lighting projects studied