Global - English

Adapting to the “new normal” with UV-C

 

April 20, 2022

 

As we learn to live with the Covid-19 pandemic, UV-C disinfection technologies can help

 

Covid-19 is here to stay. As our societies begin to open up again, we must learn to do one thing: live with the new normal. But this is difficult when cases remain high and vaccine uptake declines. We need to introduce technologies and policies that work to strengthen the protections offered by masks, social distancing, and jabs without replacing them entirely.

 

The obvious solution to living with an airborne disease is ventilation, but this can be energy-inefficient and costly, with heating bills rising as schools and offices are forced to keep windows open to encourage airflow. But because we spend much of our time living, working, and socializing indoors, buildings must be both healthy and efficient to reduce the transmission of infectious diseases. Clearly, we must improve ventilation through new engineering techniques—and that’s where UV-C comes in.

 

Ultraviolet-C is a type of radiation that breaks down the DNA and RNA of microorganisms, including viruses and bacteria, and renders them effectively harmless. The technology is a well-established method of air, water, and surface disinfection that has been offered commercially by Signify (formerly Philips Lighting) for decades. However, its true power and potential has been widely recognized only since the COVID-19 pandemic.

 

Research conducted in 2020 by the National Emerging Infectious Diseases Laboratories (NEIDL) at Boston University found that Signify’s UV-C light sources reduced SARS-CoV-2 virus infectivity on a surface to below detectable levels in as few as 9 seconds.1

Boston University has validated the effectiveness of our light sources as a preventive measure for companies and institutions as they seek ways to provide virus-free environments”

“Given the potential of the technology to aid the fight against the coronavirus, Signify will not keep the technology for its exclusive use but make it available to other lighting companies.” said Eric Rondolat, CEO of Signify.

 

Signify UV-C disinfection chambers and lamps can disinfect objects as small as handheld supermarket scanners and as large as entire buses. UV-C upper air disinfection luminaires can inactivate the virus in the upper air while people are present in the room, with features designed to shield them from potentially harmful radiation.

 

Ultimately, this means that we can bring back face-to-face teaching, business, and play.

 

Recently, the Royal Theater Carré in Amsterdam and the Theater De Ruchte in Someren have installed UV-C technology and are now welcoming patrons to public space in which they can feel confident and safe. In the Royal Theater Carré, 75 Philips UV-C upper air luminaires disinfect the building’s foyer, dressing rooms, and offices, while the Theater De Ruchte is adding another 20 luminaires to an existing pilot installation.

 

“We are just as happy as our guests and performers to be open again,” said Thomas Groen, manager of sales and partnerships at Royal Theater Carré. “Among other measures, these UV-C luminaires will minimize the risk of infection for our guests, performers, and our colleagues.”

 

Air changes per hour (ACH) is the term most commonly used to refer to the amount of outside air that needs to be introduced into an interior environment for proper ventilation. For offices and schools, the recommended ventilation level to improve ventilation and overall air quality is up to 2 ACH. However to effectively remove viruses the recommended ventilation level is 20 ACH.

 

Standard HVAC systems can be uncomfortable and costly as is, and the energy required to bring their performance up to 20 ACH would be vast. UV-C disinfection upper air luminaries overcome these limitations, disinfecting the environment and delivering the required equivalent to 20 ACH in a quiet, comfortable, unobtrusive, and energy-efficient manner.

GGD Netherlands has been equipped with UV-C disinfection devices as part of the infection prevention policy.

“I think we should use UV-C disinfection equipment more broadly,” said Roxanna van Nispen-Dobrescu, a pulmonologist at GGD Breda, the Dutch city’s municipal health service. “Before we began to use UV-C devices, some of our staff would get infected with TB by our clients. We haven’t seen any infections since we installed the luminaires as a preventative measure more than ten years ago.”

 

UV-C should—and can—complement other disease-deterrent technologies and measures. It may even increase vaccine uptake, as it can encourage individuals who may be reluctant to visit vaccinations sites for fear of catching the disease. “Some of our clients are hesitant to come in as they’re afraid of getting infected by harmful viruses or bacteria during their visit,” said Liesbeth Huizer, a medical technician at GGD Rotterdam, in the Netherlands.

 

UV-C lighting “really helps reassure them,” she added. “I’m surprised that even one and a half years into this pandemic, we’re not making broader use of a technology that we have been using for 20 years and which has proven itself against TB and SARS CoV-2. It’s such an obvious measure.”

I’m surprised that even one and a half years into this pandemic, we’re not making broader use of a technology that we have been using for 20 years and which has proven itself against TB and SARS CoV-2. It’s such an obvious measure.”

Footnotes:

 

1 Nadia Storm et al., Rapid and complete inactivation of SARS-CoV-2 by ultraviolet-C irradiation, 2020, https://www.nature.com/articles/s41598-020-79600-8. The UV-C irradiance used in this study was 0.849 mW/cm2.

About the author:

Harry Verhaar


Harry Verhaar

Head of Global Public and Government Affairs at Signify

For further information, please contact:

For editorial enquiries:

Signify Global Integrated Communications
Neil Pattie
Tel: + 31 6 15 08 48 17
Email: neil.pattie@signify.com

For commercial enquiries:

About Signify

 

Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers. We proudly bring to market the world’s best lighting brands, from Signify, Philips, Philips Hue, Signify Interact, Signify Dynalite, Color Kinetics and many more. Our advanced products, connected systems and services unlock the extraordinary potential of light for brighter lives and a better world. In 2025, we had sales of EUR 5.8 billion, approximately 27,000 employees, and a presence in over 70 markets. We are in the Dow Jones Best-in-Class World Index , earned a CDP ‘A’ score for climate performance and transparency and hold the EcoVadis Platinum rating. 

 

News and updates from Signify can be found in the Newsroom, on LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

More blogs

  • Rethinking infrastructure in highly automated data centers 

    September 21, 2026

    Rethinking infrastructure in highly automated data centers 

  • Five stadium lighting design myths busted

    August 20, 2026

    Five stadium lighting design myths busted

  • When innovation scales: Launching Philips Skylight

    June 09, 2026

    When innovation scales: Launching Philips Skylight