Unleash colors from your TV screen with new WiZ HDMI Sync Box
Eindhoven, the Netherlands – Signify (Euronext: LIGHT), the world leader in lighting is unveiling new TV sync features and products for its smart lighting brand WiZ, enabling users to effortlessly immerse themselves in a world of dynamic colors and moods. With the new WiZ HDMI Sync Box with TV backlight, users now have an easy and affordable way to sync lights to their home entertainment content, taking their movie night, sports watching and gaming time to new levels. The new Gradient Light Bars and Gradient Floor Light are designed to be the perfect addition to your TV sync experience. After being configured in the WiZ app, they will match colors to the TV screen corresponding to their physical location and create a fascinating surround lighting experience.
Bring your screen to life
The WiZ HDMI sync box with TV backlight is all that the users need for bringing their screens to life. By simply connecting the Sync box to a HDMI media device such as streaming stick, set-top box, and gaming console, and attaching the LED strip to the back of their TV, users can make lights sync with the colors and brightness of the TV screen. No need to put a camera on top of your TV screen and there is no need for a complicated calibration procedure. It supports HDMI 2.0 and video formats up to 4K at 60Hz with HDR10+/Dolby Vision. The Sync box reads the video signal directly from the HDMI input, instantly analyzes the entire screen, and generates ultra-accurate colors on the lights. Featuring a 3-side segmented RGBIC light strip for easy mounting on the back of TV, the HDMI sync box offers two different sizes, fitting TV’s from 55” to 65”, and from 75” to 85”.
The clean setup and personalized experience make the WiZ Sync Box perfect for every style and TV watching occasion. With the 4 preset sync modes - Cinematic, Vibrant, Relaxation, Rhythmic and customizable brightness, color saturation and intensity, users can set lights to closely follow all the colors with drastic brightness change or to gradually transition while matching colors to the dominant hue on the screen. The HDMI Sync Box works with any WiZ color-capable light that supports both Wi-Fi and Bluetooth. Users can link as many lights to the Sync Box as they like (they need to be connected to the same Wi-Fi network) and make them sync with TV simultaneously. The Sync Box also has a built-in microphone that can capture audio playing from any source and make lights change colors and brightness with the music. Control is simple via the WiZ app, voice (with Google or Alexa) or the WiZ remote control. Users can also set the auto-switching feature in the app so their TV sync lights will turn on and start syncing automatically whenever the HDMI media source provides a signal.
Maikel Klomp
Business Leader of WiZ Connected
Compact design, remarkable ambiance: the Gradient Light Bars
The Gradient Light Bars create captivating lighting in any space. Each light bar can be controlled individually and features a multicolor segment design that displays multiple colors simultaneously, creating beautiful wall-washing effects. Versatile in installation, the Gradient Light Bars come with various mounting brackets, allowing placement horizontally or vertically on counters or desks, or fixed behind TVs and monitors.
Bring colors to any corner: the Gradient Floor Light
The Gradient Floor light offers a multicolor segment design and wide beam angle, illuminating any room with stunning wall-washing effects. Its slim, minimalistic design fits effortlessly into any corner, complementing various interiors. Featuring a one-piece design for seamless plug-and-play functionality—no assembly required—.
Both the Gradient Light Bars and the Gradient Floor light deliver an engaging atmosphere by syncing colors with video (Sync box required) and with music. With 16 million colors and ready-to-use preset modes like Party, Fireplace, and Ocean, users can set the perfect mood for any occasion. They are Matter compatible so they can also be controlled with Alexa, Google Home and Apple HomeKit.
For more information, please visit www.wizconnected.com/explore-wiz/entertainment
Availability
Products available globally from May 2025 onwards.
HDMI sync box with TV backlight for 55”~65” TV
HDMI sync box with TV backlight for 75”~ 85” TV
Gradient Light Bars
Gradient Floor light
Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers. We proudly bring to market the world’s best lighting brands, from Signify, Philips, Philips Hue, Signify Interact, Signify Dynalite, Color Kinetics and many more. Our advanced products, connected systems and services unlock the extraordinary potential of light for brighter lives and a better world. In 2025, we had sales of EUR 5.8 billion, approximately 27,000 employees, and a presence in over 70 markets. We are in the Dow Jones Sustainability World Index and hold the EcoVadis Platinum rating.
News and updates from Signify can be found in the Newsroom, on LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

May 21, 2026
Signify included in Dow Jones Best-in-Class World Index for ninth consecutive year