You are now visiting the Signify website. A localized version is available for you.
Suggestions
    A driver is a constant current driver when it regulates the current directly for the specified range of LED voltage. Constant voltage drivers regulate a fixed voltage at the output, and the LED modules (or light engines) need to have additional on-board circuits to regulate the current in the LEDs.