The Declare Label is an initiative of the International Living Future Institute, an organization advocating for a more resilient future through the use of regenerative materials and "healthy products."
Declare is one part of Living Future's strategic plan to support harmonious living between people and the planet, and serves as a transparency platform and product database that makes it easier to find healthy products for upcoming building projects.
Declare labeling allows manufacturers to demonstrate market leadership in the growing movement toward product transparency and health in the built environment!
Find Genlyte Declare products: Declare - International Living Future Institute.

Products disclose 100% of ingredients present in the final product but contain one or more Red List chemicals that are not covered by an approved exception.
Products disclose a minimum of 99% of ingredients present in the final product and meet the LBC Red List Imperative requirements through one or more approved exceptions.
Products disclose 100% of ingredients present at or above 100 ppm (0.01%) in the final product and do not contain any Red List chemicals.
These labels are used by designers and operators to specify products they trust and meet the requirements of leading green building standards, including the Core Green Building, LBC, LEED, and WELL Certifications.
Declare labels disclose all intentionally added ingredients and residuals at or above 100ppm (0.01%) present in the final product by weight.
Each ingredient is reported with a chemical name, CAS number, and percentage or percentage range.








Between 2019 and 2024, Signify achieved a 50% reduction in absolute scope 1 and 2 greenhouse gas emissions!
1. Reduce scope 1 , 2, and 3 emissions (direct and indirect)
2. Avoid carbon emissions in the product use phase
3. Transform operations sustainably and profitably, without carbon offsets
Create engaging spaces with tunable white solutions that offer the freedom to set different ambiances in offices, schools, retail spaces, and healthcare environments.
Tunable White solutions can easily change LED intensities and correlated color temperature (CCT) from warm white (2700K) all the way to cool white (6500K). Separate control inputs for intensity and CCT ensure the color temperature remains constant when the intensity is adjusted. By adjusting the intensity of each color, the fixture can produce a wide range of color temperatures.

We spend a lot of our time indoors, often in locations without windows or proper access to daylight. Studies show that the natural light has a huge impact on productivity and alertness, reduces stress and contributes to better sleep.
NatureConnect is an advanced lighting system that reintroduces the benefits of natural light into indoor environments. Using a dynamic mix of Skylight, Daylight, and Lightscape luminaires, it creates immersive and human-centric lighting experiences that follow the body’s natural rhythm.

BioUp is a spectrally tunable technology allowing for minute adjustments to certain wavelengths in the LED light spectrum. By enhancing the LED spectrum with cyan light, BioUp helps to support biological impact. You may not see the impact of BioUp on the visual color or intensity of light, but you can experience the impact on how you feel and perform.