Norge - Norsk

Philips Lighting’s new innovations make switching to LED lighting even easier

March 13, 2018

Eindhoven, the Netherlands – Philips Lighting (Euronext: LIGHT), the world leader in lighting, today announced two new innovations, the Philips TrueForce LED Road and the Philips CorePro LEDtube Universal T8. Philips TrueForce LED Road is the world’s first ‘plug and play’ replacement SON-T LED lamp for street lighting, making it easy to upgrade existing installations to LED without having to replace the luminaire. The Philips CorePro LEDtube Universal T8 is a breakthrough range of affordable tubes for trade customers, making tube replacement as easy as it was with fluorescent tubes.

 

Philips TrueForce LED Road for ‘like-for-like’ street lighting

The new Philips TrueForce LED Road is the first of its kind to fit into the standard E27 fixture and replicate a similar light effect to conventional street lighting. Philips TrueForce LED Road reduces the time needed to maintain, replace and fit each street light, including the knock-on time required for road closures. In addition, its longer lifespan of more than eight years plus energy savings of up to 45% compared to conventional bulbs help save on running costs.

 

The Nacka Municipality in Sweden has already trialed the new Philips TrueForce LED Road. Mikael Jansson, the street lighting expert at the municipality said: “Philips TrueForce LED Road, provides better light quality and a safer outdoor environment, compared to a 70W high pressure sodium lamp. The installation was as easy as installing a regular lamp and it fit various distinctive applications. Philips TrueForce LED Road is a good alternative to LED luminaires when budgets are tight.”

 

Modernizing the traditional 20-30-year old street lighting design, the new Philips TrueForce LED Road distributes a similar amount of light as conventional street lights and is available in warm white as well as a cooler white, to seamlessly blend in with existing street lights. With a significantly improved Color Rendering Index compared to conventional SON-T lamps, it also enhances the feeling of comfort and safety. Philips TrueForce LED Road will be available across Europe from July 2018.

 

Philips Lighting Strengthens Universal LED Tubes Portfolio with New Affordable Range for Trade Customers

Philips Lighting announced a breakthrough range of universal tubes, the Philips CorePro LEDtube Universal T8, for trade customers. With this new addition, Philips Lighting now offers the broadest range of LED tubes for different applications in the industry, serving the high-end specification market with the existing MASTER Universal range and trade customers with the new CorePro Universal range.

 

Harnessing Philips Lighting`s expertise, Philips CorePro LED tube Universal T8 makes installing tubes as easy as it used to be with fluorescent tubes. The range is affordable compared to high end universal LED tubes, making it the ideal alternative to standard fluorescent lights for trade customers.

 

Designed for simplicity, the Universal T8 tube is optimized to work with all driver technologies, fitting directly in luminaires operating on electromagnetic ballasts or HF electronic ballasts, reducing the cost of stocking different types of tubes. Philips CorePro LED tube Universal T8 can also connect directly to the mains power, bypassing the ballast. This enables additional energy savings. And by simplifying the tube selection process, it enables lighting professionals to allocate their time, expertise and resources to installing the perfect lighting for different needs.

 

Designed for lighting a wide variety of spaces like car parks, garages, corridors and shopping malls, the new universal LED tube delivers a high quality and reliable light along with up to 65% energy-savings, compared to the traditional TL-D fluorescents it replaces. Philips CorePro LEDtube Universal T8 will be available across Europe from May 2018.

 

Philips Lighting will be showcasing its new LED lamps at Light+Building 2018, at the Philips Lighting booth in Hall 0: Forum. Media and bloggers are invited to join the Philips Lighting press conference, on Monday, March 19, at 1.00pm at the Philips Lighting booth. You can also watch the press conference webcast live Click here.

Philips CorePro LEDtube Universal T8 
Product type
Lumen Output
Operations
Beamangle
CRI
Color temp.
Lifetime
Energy label
Im
IM/W
°
-
K
Hrs.
-

CorePro LEDtube UN 1200mm HO 18W830 T8

1850
EM & Mains & HF
240
80
3000
30.000
A+
CorePro LEDtube UN 1200mm HO 18W840 T8
2000
EM & Mains & HF
240
80
4000
30.000
A+
CorePro LEDtube UN 1200mm HO 18W865 T8
2000
EM & Mains & HF
240
80
6500
30.000
A+
CorePro LEDtube UN 1500mm HO 23W830 T8
2500
EM & Mains & HF
240
80
3000
30.000
A+
CorePro LEDtube UN 1500mm HO 23W840 T8
2700
EM & Mains & HF
240
80
4000
30.000
A+
CorePro LEDtube UN 1500mm HO 23W865 T8
2700
EM & Mains & HF
240
80
6500
30.000
A+
Philips TrueForce LED Road
Product type
Lamp Wattage
System Wattage
Lumen output
Color temp.
Life-time
W
CRI
Surgey protection
Dimensions
W
W
Im
K
Hrs.
-
kV
D x L
TForce LED HPS ND E27 740
37
46
6000
4000K
50.000
70
6kV
60 x 196
TForce LED HPS ND E27 730
37
46
5500
3000K
50.000
70
6kV
60 x 196

For further information, please contact:

Philips Lighting Global Communications

Bengi Silan Genc

Tel: +31 6 25 44 17 98

E-mail: bengi.genc@signify.com

About Philips Lighting

Philips Lighting (Euronext: LIGHT), the world leader in lighting products, systems and services, delivers innovations that unlock business value, providing rich user experiences that help improve lives. Serving professional and consumer markets, we lead the industry in leveraging the Internet of Things to transform homes, buildings and urban spaces. With 2017 sales of EUR 7.0 billion, we have approximately 32,000 employees in over 70 countries. News from Philips Lighting is located at the NewsroomTwitter and LinkedIn. Information for investors can be found on the Investor Relations page.