Suggestions

    Signify and Boston University validate effectiveness of Signify’s UV-C light sources on inactivating the virus that causes COVID-19

    June 16, 2020

     

    • Test results show that the virus could no longer be detected after seconds of exposure
    • Signify to make its UV-C lighting technology widely available to other lighting companies
    • Signify has been at the forefront of UV technology for more than 35 years

     

    Eindhoven, the Netherlands Signify (Euronext: LIGHT), the world leader in lighting, together with the National Emerging Infectious Diseases Laboratories (NEIDL)1 at Boston University in the US have conducted research that validates the effectiveness of Signify’s UV-C light sources on the inactivation of SARS-CoV-2, the virus that causes COVID-19.

     

    Since the start of the SARS CoV-2 pandemic, Dr. Anthony Griffiths, Associate Professor of Microbiology at Boston University School of Medicine and his team have been working on developing tools to support scientific advancement in this field.2 During their research they have treated inoculated material with different doses of UV-C radiation coming from a Signify light source and assessed the inactivation capacity under various conditions. The team applied a dose of 5mJ/cm2, resulting in a reduction of the SARS-CoV-2 virus of 99% in 6 seconds. Based on the data, it was determined that a dose of 22mJ/cm2 will result in a reduction of 99.9999% in 25 seconds.3

    Our test results show that above a specific dose of UV-C radiation, viruses were completely inactivated: in a matter of seconds we could no longer detect any virus.”

     

    Dr. Anthony Griffiths

    Associate Professor of Microbiology at Boston University School of Medicine 

    “We’re very excited about these findings and hope that this will accelerate the development of products that can help limit the spread of COVID-19,” he added.

     

    Signify is the leader in UV-C light sources and has been at the forefront of UV technology for more than 35 years. It has a proven track record of innovation in UV-C lighting, which is designed, manufactured and installed in line with the highest safety standards.

    I’m very happy about the fruitful cooperation with Boston University in the fight against the coronavirus. Boston University has validated the effectiveness of our light sources as a preventive measure for companies and institutions as they seek ways to provide virus-free environments.”

     

    Eric Rondolat

    CEO of Signify

    “Given the potential of the technology to aid the fight against the coronavirus, Signify will not keep the technology for its exclusive use but make it available to other lighting companies. To service the growing need for disinfection we will increase our production capacity multifold in the coming months,” he added.

     

    1 The NEIDL is a state-of-the-art research facility that encompasses significant containment laboratories at Biosafety Level -2, -3, and -4

    2 Dr. Griffiths’ team develops vaccines and therapeutics for Risk Group 3 and 4 viruses, which include organisms that can cause serious or deadly diseases in humans

    3 Research variables are available upon request

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2023, we had sales of EUR 6.7 billion, approximately 32,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for seven consecutive years and have achieved the EcoVadis Platinum rating for four consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

    Meydan Bridge

    More press releases

    • Share repurchase program completion

      May 16, 2024

      Share repurchase program completion

    • Signify shareholders approve all AGM 2024 proposals

      May 14, 2024

      Signify shareholders approve all AGM 2024 proposals

    • Repurchase program to cover performance share plans

      April 29, 2024

      Repurchase program to cover performance share plans