Making the city work for you with Traffic Adaptive Lighting

For more than a century, public lighting has served a simple purpose: illuminate streets after dark. However, cities are not static environments. Traffic patterns fluctuate by the minute, weather conditions shift unexpectedly, and urban activity increasingly operates around the clock. In this context, lighting systems that follow fixed schedules are becoming an outdated infrastructure model.

 

So, the next evolution is not brighter lighting. It is smarter lighting that learns the city and responds to its needs.

 

Adaptable lighting represents a fundamental shift by leveraging real-time and predictive data, such as traffic flow and weather conditions—lighting systems can dynamically adjust illumination levels based on actual need rather than assumptions made months or years earlier. Let’s dive in.

What is Traffic adaptive lighting

 

In a crux, traffic adaptive lighting is technology that learns the city.

 

Cities are dynamic. Traffic changes, weather shifts, and conditions evolve throughout the night. Yet most street lighting still relies on fixed schedules, creating a gap between planned lighting and real-world conditions. Adaptable Lighting use real-time and predictive data on traffic flow to inform lighting strategies—helping cities align lighting with actual conditions, optimise operations, and reduce energy use.

 

Traffic Adaptive Lighting (TAL) is an intelligent street lighting solution designed to reduce energy consumption and carbon emissions by dynamically adjusting lighting levels in response to real time traffic conditions. Unlike traditional fixed‑output street lighting, TAL uses live vehicle count data and environmental inputs to tailor illumination to actual road usage throughout the night.

 

Traffic Adaptive lighting is the adjustment of lighting based on the current conditions of the highway/road.

 

The following parameters can change through the night and can influence the lighting level required to maintain safety:

  • Traffic volume.
  • Pedestrian and bicycle presence.
  • Parked vehicles.
  • Ambient conditions.
  • Pedestrian safety and security.
  • Road conditions.
  • Weather conditions.

 

Allowing the lighting output to be changed based on real time conditions. The solution was developed to not only reduce the energy and carbon consumption associated with streetlighting, but to also provides better visibility for road users with lighting which can be adapted on event days (near football stadium), and the waterfront area, while also providing a more resilient infrastructure with quicker repair cycles.

 

Liverpool shining

 

Like many cities, Liverpool faces the challenge achieving Net Zero by 2030 with a focus on reducing energy demand and enabling a cleaner infrastructure while supporting a thriving fair and sustainable city.  Highways assets have a role to play in reducing operational carbon and in a move towards smart, data-driven infrastructure, Liverpool City Council, in collaboration with McCann, Signify and Upciti, has implemented Traffic Adaptive Lighting system, positioning Liverpool as a leader in smart city innovation.

 

The installation covers two key routes on the A565 linking the city centre to the new Hill Dickinson Stadium, home to Premier League club Everton FC and other major events.

 

This pilot project is funded by ADEPT Live Labs 2 Decarbonising Local Roads, a three-year, UK-wide £30 million programme funded by the Department for Transport that aims to decarbonise the local highway network.

 

Benefits to the city: The lighting can bring upto 30% in energy savings over the next 10 years. The city also needed to increase safety for pedestrians on match days as routes leading to Everton Stadium experience significant surges in traffic during events, requiring brighter, adaptive lighting for safety and crowd management. In addition, in the past, the council has relied on public reports to identify lighting failures, leading to delays in repairs and potential safety risks. As budgets tighten and energy costs rise, the city is pursuing innovative, efficient ways to invest in the future.

 

/content/dam/signify/en-gb/blog/business/traffic-adaptive-lighting/liverpool-shines.jpg

 

What’s behind the system

 

The system uses Signify LumiStreet Gen2 ZD4i certified luminaires which are connected to the Signify Interact City central management system, and which in turn is linked via APIs to Upciti's privacy-by-design urban sensors, providing real-time mobility data.

 

The sections on the A565 of Great Howard Street and Derby Road are of a similar profile with lengths of urban dual carriageway separated by kerbed central reservation and have a high density of both controlled and uncontrolled junctions and pedestrian crossing areas. Parking is controlled for most of the route, but there are a number of in-lane bus stops in both directions.

 

The new lighting scheme has been designed to M2 lighting class for the event lighting and a reduced class for all other times.  Based on the historical Average annual daily traffic flows (AADT) of 17000-20000 vehicles.  Considering the complexity of the visual navigation task, It is expected that the Lighting class during peak periods will be M3, with the option reduce to an M4 lighting class in low traffic conditions as per ILP PLG08 Guidance on the application of adaptive Lighting. As per BS5489 – 2020, subject to risk assessment the lighting could be further reduced to M5 after final bus services and pedestrian use of the area also reduces in the early morning hours.

 

The four Upciti sensors provide real-time mobility insights, enabling lighting levels to automatically adapt to changing traffic conditions. The result is improved energy efficiency without compromising safety or visibility.

 

/content/dam/signify/en-gb/blog/business/traffic-adaptive-lighting/liv-upciti-sensor-image.jpg

Cities need trusted, privacy-by-design infrastructure capable of turning real-time mobility data into action. By delivering actionable insights without recording or transmitting identifiable images, our multi-use sensors help cities improve safety, reduce energy consumption, and optimize public services, to help build smarter and more sustainable urban environments."

 

Elie EL KHOURY,

International Business Development Manager & Sales Director, Upciti

At the centre of the project is Signify’s Interact City lighting control system, which continuously monitors performance and automatically detects faults to minimise downtime and maintenance costs. This proactive approach enhances public safety and streamlines management of lighting assets across the waterfront area. Interact City connects both new and existing luminaires, creating a unified lighting network that reduces energy use and supports future citywide upgrades.

 

On high-demand days, such as matchdays at Everton’s nearby stadium, Liverpool City Council can respond more effectively to increased requirements for lighting, operational efficiency and public safety. Lighting levels can be increased to maintain optimal visibility and support safer public spaces.

 

With each luminaire connected to Signify’s central management platform, the council can proactively manage the lighting network using real-time data and insights. This smart approach helps minimise energy waste by ensuring lighting is only used when and where it is needed, avoiding the inefficiencies of fixed schedules that can create a disconnect between planned lighting and actual conditions.

 

We’re proud to be among the first UK local authorities to deploy traffic-adaptive lighting at scale. This investment is helping us reduce energy consumption, improve operational efficiency, and build a more sustainable, future-ready city. The upgrade responds to the evolving needs of residents while supporting the ambitions of a growing city, delivering smarter infrastructure that enhances safety, efficiency, and the overall urban environment for everyone.”

 

Ali Zahran

Principal Street Lighting Engineer at Liverpool City Council

Since the Hill Dickinson Stadium opened, we’ve listened closely to fans who want a safe, well lit route back towards the city centre and key transport links. The new adaptive lighting along the busiest roads around the stadium means pavements are brightly lit when people need it most, helping everyone feel safer as they move through the area. Because the system responds in real time, we can also spot and fix faults quickly, keeping the route reliably lit on matchdays and beyond. And by adjusting the lighting to actual traffic levels, we’re cutting unnecessary energy use and delivering real savings for the city.”

 

Councillor Dan Barrington, 

Cabinet Member for Transport and Connectivity

In conclusion

 

The smartest cities of the next decade will not be defined by the number of sensors they deploy or the amount of data they collect. They will be defined by how effectively they convert information into action.

 

Adaptable lighting offers a glimpse of that future: infrastructure that observes, understands, and responds in real time. The streetlight is no longer just a source of illumination; it is now a node in an intelligent urban ecosystem. And that may be one of the most important shifts in city infrastructure since the invention of electric light itself.

 

As Liverpool leads the way for smart innovation, this sets the stage for how cities can respond to citizen needs.

 

About the author:

Mario Giordano

Michael Wilkinson

Sales System Architect

For further information, please contact:

Signify UK&I PR

Nikita Mahajan
Tel: + 44 (0)7459751618
Email: nikita.mahajan@signify.com

 

About Signify

 

Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers and lighting for the Internet of Things. Our Philips products, Interact connected lighting systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2022, we had sales of EUR 7.5 billion, approximately 35,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We achieved carbon neutrality in our operations in 2020, have been in the Dow Jones Sustainability World Index since our IPO for six consecutive years and were named Industry Leader in 2017, 2018 and 2019. News from Signify is located at the Newsroom, Twitter, LinkedIn and Instagram. Information for investors can be found on the Investor Relations page.

Meydan Bridge

More blogs

  • Emergency Lighting: Why It’s a Real Business Asset

    October 28, 2026

    Emergency Lighting: Why It’s a Real Business Asset

  • Measuring the Value of Architectural Lighting Design

    September 10, 2026

    Measuring the Value of Architectural Lighting Design

  • GreenSpace Perfect Fit: The Future of Seamless Lighting Renovation

    June 21, 2026

    GreenSpace Perfect Fit: The Future of Seamless Lighting Renovation