Designing for a world beyond standard lighting: why “GreenSpcae perfect fit” signals the future of renovation

Lighting renovation has long been defined by compromise. Installers and designers typically work within the constraints of legacy ceiling cut-outs, outdated fittings, and fragmented product catalogues. The result is familiar: adapter rings, visible mismatches, and time-consuming searches for “close enough” replacements.

 

The perfect fit concept from Signify myCreation challenges that entire paradigm by reframing what a retrofit solution should be: not an approximation, but a precision-designed match. Something that seamlessly fits, does not look like a replacement and feels like a part of the ‘setting’.

 

Signify myCreation perfect fit is part of a broader shift towards custom, on-demand, 3D-printed lighting systems that are engineered around real-world renovation constraints rather than forcing buildings to conform to standardised products. The benefits are many. Let’s dive in.

From replacement to reconfiguration

 

Traditional lighting upgrades typically start with a product catalogue. 3D printed lighting flips that approach: it starts with the physical space.

 

Instead of selecting from a limited range of diameters, trims, or mounting solutions, installers can configure a downlight that is designed to integrate seamlessly into existing ceiling conditions. This removes one of the most persistent pain points in refurbishment projects: the mismatch between old infrastructure and new lighting technology. The outcome is a shift from replacement thinking to system reconfiguration where the fixture adapts to the building, not the other way around.

 

Cleaner aesthetics, simpler installation

 

One of the most visible benefits of perfect fit is aesthetic continuity. By eliminating the need for adapter rings and workaround fittings, ceilings maintain a uniform, architectural finish. But the value proposition extends beyond just design. Installation complexity is reduced significantly, as the solution is engineered to integrate directly into the intended retrofit environment. In practice, this means fewer components, less on-site adaptation, and faster deployment cycles.

 

The luminate also offers a variety of optics for comfort and task lighting, as well as ambiance (with multiple color and texture options) to go along with the broad lumen ranges, enabling use from small rooms to high ceilings, so one product for multiple spaces (faster renovation/less disruption).

cleaner-aesthetics-image Office room

Sustainability through precision manufacturing

 

Perfect fit also reflects a broader industrial transition: manufacturing only what is needed, when it is needed, rather than having to order a minimum quantity. The 3D printing approach aligns production directly with project specifications, producing the exact quantity needed and what more, the luminaire is easy to upgrade, with components that can be replaced without tools.

 

As part of Signify myCreation’s 3D printing approach, luminaires are produced on demand using high levels of recycled and bio-circular materials. This reduces excess inventory, minimises waste, and supports a more circular production model.

 

A step toward circular renovation practices

 

Renovation is one of the most resource-intensive activities in the built environment. Pprfect fit contributes to reducing that footprint in two ways:

 

  • By extending the usable life of existing ceiling infrastructure through precise adaptation
  • By reducing material waste through additive, on-demand manufacturing

Together, these changes point toward a more circular approach to building upgrades where renovation does not necessarily mean replacement, but intelligent adaptation.

Intelligence Integrated

 

The perfect fit comes with Integrated intelligence features, including daylight sensing, automatically adjust light output when sufficient natural light is available, reducing unnecessary energy consumption. Presence detection further enhances efficiency by dimming or switching off lights in unoccupied spaces. Because these smart functions are built directly into the system, there is no need for external sensors, helping to maintain clean ceiling aesthetics while simplifying installation. The result is instant energy savings, improved convenience, and a smarter approach to lighting control.

 

In action at El Dorado Airport

 

As part of their strategy against climate change, the International Airport Operator (OPAIN) was looking for a solution to mitigate the impact of their activities and reduce their carbon footprint. Their maintenance department, together with other areas of the airport, constantly adopt measures aimed at increasing the efficiency of the airport’s infrastructure, which covers an area of approximately 6.9 km². The main aim of their initiative was to retrofit interior luminaires whilst making sure lighting has the least possible negative impact.

 

Given that terminals are 24/7 transit points, the priority was to offer greater visual comfort for passengers and better workspaces for the entire airport workforce. For outdoor lighting, the challenge was to implement a cloud-based system that allowed them to manage operations and maintenance remotely with maximum reliability and safeguards. El Dorado is the first project of its kind in Latin America to implement the latest innovation in lighting both by using 3D printed luminaires and Interact City systems to remotely manage exterior lights.

conference room

In Conclusion

 

Perfect fit is less about a single product and more about a design philosophy: that renovation should not require compromise. By aligning manufacturing precision with real-world installation conditions, it points toward a future where lighting systems are seamlessly integrated, sustainably produced, and inherently tailored to the spaces they inhabit. Say goodbye to frustrating refits! Your apeture, perfectly matched. Every time.

About the author:

Justine walmsey

Justine Walmsley

Marketing Communications Specialist

For further information, please contact:

Signify UK&I PR

Nikita Mahajan
Tel: + 44 (0)7459751618
Email: nikita.mahajan@signify.com

 

About Signify

 

Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers and lighting for the Internet of Things. Our Philips products, Interact connected lighting systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2022, we had sales of EUR 7.5 billion, approximately 35,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We achieved carbon neutrality in our operations in 2020, have been in the Dow Jones Sustainability World Index since our IPO for six consecutive years and were named Industry Leader in 2017, 2018 and 2019. News from Signify is located at the Newsroom, Twitter, LinkedIn and Instagram. Information for investors can be found on the Investor Relations page.

Meydan Bridge

More blogs

  • Emergency Lighting: Why It’s a Real Business Asset

    October 28, 2026

    Emergency Lighting: Why It’s a Real Business Asset

  • Measuring the Value of Architectural Lighting Design

    September 10, 2026

    Measuring the Value of Architectural Lighting Design

  • GreenSpace Perfect Fit: The Future of Seamless Lighting Renovation

    June 21, 2026

    GreenSpace Perfect Fit: The Future of Seamless Lighting Renovation