St. Laurentii
Söderköping, Sweden
With LED lighting and lighting scenarios, St. Laurentii church in Söderköping has obtained an effective church space that can be adapted to different needs. Church visitors now have, with the help of light and sound, the opportunity to experience different moods, for example feeling uplifted, reflecting or meditating. For the lighting effects, quality and reliability were important, and the luminaires were discrete. ColorGraze RGBW, which offers a wide range of optical solutions, was the perfect luminaire for the effect lighting and was mounted on the floor to illuminate the arches and columns of the church. The headlamps were also replaced by spotlights with Philips Master LED AR111 on 11W, increasing the power to 5,000W, instead of the previous 1,100W. The Philips Dynalite control system has been used for all church lighting and has been combined with the iPlayer 3 control system and Color Kinetics products to create a total effect lighting solution. Since the LED products have a long life time, St. Laurentii church saves a lot on maintenance. The church has received a very effective lighting which highlights the architecture of the church room with sustainable products that draw some energy and last a long time.