Australia - English

Philips Dynalite launches AntumbraTouch user interface in Australia and New Zealand

September 16, 2013

Sydney, Australia - Philips Dynalite has released AntumbraTouch, the anticipated second user interface design in its Antumbra range for networked control systems used in high-end residential, hospitality and commercial market segments.

 

The new AntumbraTouch has a smooth glass finish and uses ‘capacitive touch’ technology to detect the presence of a finger on various locations of the glass to trigger the button-press action, similar to that of a smart phone interface.

 

Like the AntumbraButton user interface, the AntumbraTouch panel can be custom configured to have different button combinations and perform a vast range of functions that enable users to create local lighting scenes, monitor temperature and manage site-wide networked devices such as blinds and HVAC systems.

The architecturally minimalist Antumbra panel features hidden sensory inputs including proximity sense, light level sense, and finally temperature sense for control of the local environment and to reduce the need for additional unsightly temperature sensors.

 

Using the latest in ‘field-effect technology’, the panel is able to detect a user’s presence and will ‘light up’, resulting in a wall wash effect welcoming the user to interact with the device.  When the user moves away, the light wash effect around the panel fades away, allowing the panel to merge into the wall architecture.

 

To ensure the Antumbra range sets the standard for user interfaces from both a design and an engineering perspective, Philips Dynalite took a collaborative approach to development, consulting widely with customers and the channel network.   As a result of this approach, the AntumbraButton product design was recently recognised by the ADIA with a 2013 Design Award.

 

A range of different finish options are available to suit any interior. AntumbraTouch fascias are available in black or white and can be combined with black, white, aluminium or chrome rim colours. 

 

An additional graphical display user-interface panel will be added to the Antumbra range later in 2014.

 

Antumbra is available from accredited Philips Dynalite resellers only.

Image-1

Image-1

The new AntumbraTouch features a smooth glass finish and uses ‘capacitive touch’ technology to detect the presence of a finger on various locations of the glass to trigger the button-press action.

Image-2

Image-2

Using the latest in ‘field-effect technology’, the AntumbraTouch panel is able to detect a user’s presence and will ‘light up’, resulting in a wall wash effect welcoming the user to interact with the device.  When the user moves away, the light wash effect around the panel fades away, allowing the panel to merge into the wall architecture.

For further information, please contact:

Katherine Cammuso
FleishmanHillard
Tel: +61 2 9025 9233
Email: katherine.cammuso@fleishman.com.au

.

About Royal Philips

Royal Philips (NYSE: PHG, AEX: PHIA) is a diversified health and well-being company, focused on improving people’s lives through meaningful innovation in the areas of Healthcare, Consumer Lifestyle and Lighting. Headquartered in the Netherlands, Philips posted 2012 sales of EUR 24.8 billion and employs approximately 115,000 employees with sales and services in more than 100 countries. The company is a leader in cardiac care, acute care and home healthcare, energy efficient lighting solutions and new lighting applications, as well as male shaving and grooming and oral healthcare. News from Philips is located at www.philips.com/newscenter.

.