India - English
The Citizen House in Odense

The Citizen House in Odense

Municipality of Odense, Denmark

A participatory process actively involving citizens resulted in the creation of a dynamic and lively centre. Thanks to a gold finish and the use of light, the building has become an attractive meeting point. 

The architecture of the Citizens' House is designed for its users – thanks to the use of gold, light and, most importantly, citizens' involvement in defining the concept. During the day, the golden façade glows under natural light, and at night, it is illuminated by LED recessed lights made with special eW Graze QLX Powercore luminaires. The drama of the golden exterior is matched internally by a large empty space whose main point of interest is a sculptural staircase known as the Harry Potter Staircase. It is a point of reference and orientation for anyone moving through the Citizens' House. The architects had a clear idea that the building was not designed to be observed from outside, but to be used from inside.

Team

AI Architects Engineers, Henry Jensen A/S, Bravida, Claus Løgstrup, Signify Danmark

The Citizen House in Odense
Stairs in The Citizen House in Odense
Outside view of The Citizen House in Odense
Multiple stairs - The Citizen House in Odense