United Kingdom - English

Philips and St Helens Shape Energy-Efficient Strategy for Europe

June 6, 2011

Merseyside, UK- Philips is working with St Helens Council to trial LED street lighting in St Helens, Merseyside - as part of the pan-European BLISS project – to help shape an energy-efficient street lighting strategy for Europe.

 

The BLISS (Better Lighting in Sustainable Streets) project is designed to evaluate a wide range of options for making street lighting more energy efficient. It is part-funded by the European Regional Development grant funded from the North West Europe INTERREG IVB investment programme and currently includes projects in the UK, Netherlands, Belgium and Germany.

 

In the UK, two areas were selected for the trials; Coronation Drive Estate in Haydock to assess and compare different options for residential street lighting, and Tithebarn Road in Billinge, to investigate the effectiveness of LED road lighting. The project was implemented as a joint partnership between St. Helens Metropolitan Borough Council and Philips Lighting.

 

Rory Lingham, Assistant Director (Engineering) with the Council, explained: “The key to our proposal is to develop a range of socially acceptable energy-reducing solutions whilst considering their wider social and economic impacts in terms of public perception, crime, accident and economic regeneration. We believe we can create new low-energy lighting solutions which offer greater comfort, safer environments and improve everyday urban life.”

 

Coronation Drive Estate

 

The purpose of the Coronation Drive element of the project was to create an environment where different types of street lighting could be easily compared with each other simply by walking from one street to another. The key comparisons, from both a performance and perception point of view, were between new LED lighting and more traditional light sources.

 

To that end, one street uses low pressure sodium (SOX) light sources, another uses high pressure sodium (SON) and a third uses Philips CosmoPolis ceramic discharge metal halide lamps. In addition, Philips SpeedStar street lanterns have been installed in three streets, each with different colour temperatures - 3,000K, 4,000K and 5,600K.

 

“The new lighting is of a much higher standard. It enables people to recognise colours and see objects much more clearly than the lighting which was there before,” Rory Lingham observed.

 

Tithebarn Road

 

Tithebarn Road is a 1km stretch of 60 mph road that links two areas of St Helens. The road was originally lit by 23 x 8m columns using a mixture of low and high pressure sodium light sources.

 

The older lighting has now been replaced with 20 x 10m columns using Philips SpeedStar LED lanterns. The higher light output of the new lanterns has enabled fewer, taller columns to be used to maintain the required light levels and light distribution. In addition, controls have been introduced to dim the lighting to 50% between midnight and 6am.

 

“We believe this was the first full-scale demonstration of the SpeedStar lighting in the world. The quality of the lighting is much improved and that’s a real advantage to motorists. It’s now much easier to see other vehicles and pedestrians on the road,” Rory Lingham noted.

 

As a result of these changes, energy consumption for this stretch of road has been reduced by 21%, saving approximately 1,145kg of carbon emissions per annum. The Council will also benefit from a considerable reduction in maintenance costs due to the much longer life of the LED light sources.

 

 “The BLISS project has resulted in considerable reductions in energy consumption. Moreover, the public has shown great acceptance of what we’ve done. The survey has shown that around 78% prefer the whiter light of the LEDs. And, because we are also getting 25-50% energy savings it makes sense to install LEDs in these sorts of areas,” Rory Lingham concluded.

Further information

For further information, please contact:

 

Media Relations Manager

Philips Electronics, Corporate Communications UK
Barbara Neate Tel; +44 1483 293 071

barbara.neate@signify.com

 

About Royal Philips Electronics

Royal Philips Electronics of the Netherlands (NYSE: PHG, AEX: PHI) is a diversified health and well-being company, focused on improving people’s lives through timely innovations. As a world leader in healthcare, lifestyle and lighting, Philips integrates technologies and design into people-centric solutions, based on fundamental customer insights and the brand promise of “sense and simplicity.” Headquartered in the Netherlands, Philips employs about 117,000 employees with sales and services in more than 100 countries worldwide. With sales of EUR 22.3 billion in 2010, the company is a market leader in cardiac care, acute care and home healthcare, energy efficient lighting solutions and new lighting applications, as well as lifestyle products for personal well-being and pleasure with strong leadership positions in male shaving and grooming, portable entertainment and oral healthcare. News from Philips is located at www.philips.com/newscenter.