Seeing the difference: how lighting can lift health and wellbeing on the factory floor

 

Walk onto almost any production floor and you will find a workforce under pressure. Lines run longer, shifts stretch around the clock, and tasks demanding precision from the first hour to the last. Manufacturers rightly focus on ergonomics, PPE and training to protect their people. But one factor is present in every task, every shift and every corner of the facility, and one that must not be an afterthought: light.

 

Lighting is usually specified to meet a standard and then forgotten until a fitting fails. That mindset misses an opportunity. The quality of light shapes how well people see hazards, how tired their eyes become, how alert they feel at 3am and, how they feel about coming to work and ultimately, how well they perform a task. Getting it right is not only an operational decision; it is a wellbeing decision.

Safety starts with seeing clearly

 

The most immediate link between lighting and wellbeing is safety. Dim aisles, shadowed workstations, glare off reflective surfaces and fittings that flicker or fail all raise the risk of an incident. The case for doing better is compelling: one logistics operator reduced accidents by 14% after improving its lighting.

 

Uniform, glare-controlled LED lighting is the foundation, but connected lighting goes further. When luminaires report their own status, a failed fitting is flagged on a dashboard immediately rather than discovered by someone working in the dark. Maintenance can be planned using lifetime data before light levels drop, which also means fewer unplanned trips up ladders and lifts in busy production areas. At Pilkington's historic glass plant, connected lighting gave the team visibility and control across the whole factory, improving working conditions while reducing downtime.

The right light for the task, and the person

 

Manufacturing is not one environment but many. An inspection bench, an assembly line, a goods-in bay and a breakroom place very different demands on the eye. A single flat light level is a compromise that serves no one particularly well.

 

Driven by connected lighting, scene management is another feature that lets facility teams deliver the right light at the right time: crisper, brighter light for detailed inspection; balanced light for general production; softer settings in rest areas where people need to switch off properly. Schedules can follow the rhythm of shifts, and unoccupied zones can be dimmed without leaving anyone working in gloom.

Solar hybrid lighting Edinburgh

Supporting the body clock on every shift

 

For many manufacturers, operations never stop. Night and rotating shifts put real strain on the body's internal clock, affecting sleep, alertness and long-term health. Lighting cannot remove that strain, but it can help. Circadian lighting, which adjusts intensity and colour temperature across the day and night, is designed to work with people's natural rhythms rather than against them. For a workforce that may see little daylight during a shift, that is a meaningful step towards a healthier workplace.

Solar hybrid lighting Edinburgh

Beyond light: a healthier building

 

Because luminaires are spread throughout a building, they make an ideal backbone for sensing. Embedded sensors can monitor occupancy and environmental conditions, giving managers the data to spot risks and reduce the likelihood of accidents. Through open APIs, lighting can be integrated with HVAC, emergency systems and building management platforms such as BACnet, so comfort, air and light are managed together rather than in silos. Movement data can also reveal congestion points, helping planners design layouts that keep people and vehicles safely apart.

Wellbeing and sustainability go hand in hand

 

It is sometimes assumed that investing in people and cutting costs pull in opposite directions. With lighting, they align. Managed LED lighting can deliver energy savings of up to 80%, freeing budget and supporting decarbonisation targets while improving the quality of light on the floor. When Dubai Electricity and Water Authority upgraded its Jebel Ali power stations to efficient LED lighting, it improved visibility and working conditions while lowering maintenance.

 

At Signify, we see three challenges recurring across industrial sites: the pressure to digitalise, the need to protect employee safety and wellbeing, and the drive towards sustainability. Connected lighting addresses all three. It can start simply, with a switch to high-quality LED, and scale as needs evolve, adding data-driven capabilities when the business is ready.

Putting people at the centre

 

At Signify, we see three major challenges for manufacturers: the pressure to digitalise, the need to protect employees, and the drive towards sustainability. Connected lighting addresses all three. It can start simply, with a switch to high-quality LED, and scale as needs evolve.

 

The factories of the future will be more automated and more data-driven, but they will still depend on skilled people who can see clearly, stay alert and feel valued. Lighting is one of the few investments that touches every one of them, on every shift. Manufacturers who treat it as part of their health and wellbeing strategy, rather than a line on the maintenance budget, will create workplaces where people are safer, more comfortable and better able to do their best work.

 

The question for manufacturing leaders is no longer whether lighting matters to their people. It is whether their lighting is working as hard for their people as their people work for them.

About the author:

Clark Morrow

 

Clark Morrow
Channel & Segment Manager, Professional lighting, Signify UK&I

About Signify

 

Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers and lighting for the Internet of Things. Our Philips products, Interact connected lighting systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2022, we had sales of EUR 7.5 billion, approximately 35,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We achieved carbon neutrality in our operations in 2020, have been in the Dow Jones Sustainability World Index since our IPO for six consecutive years and were named Industry Leader in 2017, 2018 and 2019. News from Signify is located at the Newsroom, Twitter, LinkedIn and Instagram. Information for investors can be found on the Investor Relations page.

Meydan Bridge