Australia - English

Unleash colors from your TV screen with new WiZ HDMI Sync Box

July 18, 2025

Unleash colors from your TV screen with new WiZ HDMI Sync Box

  • WiZ announces the global launch of the HDMI Sync Box with TV Backlight, making it easier than ever to enjoy an immersive movie, sports watching, and gaming experience.
  • The HDMI Sync Box reads signals directly from video source and generates ultra-accurate colour effects to make your lights match the on-screen colours in real time.
  • Elevate your TV experience by linking the new Gradient Light Bars and Gradient Floor light to the HDMI Sync box, creating wall washing effects in perfect sync with the TV.

 

Eindhoven, the Netherlands – Signify (Euronext: LIGHT), the world leader in lighting is unveiling new TV sync features and products for its smart lighting brand WiZ, enabling users to effortlessly immerse themselves in a world of dynamic colours and moods. With the new WiZ HDMI Sync Box with TV backlight, users now have an easy and affordable way to sync lights to their home entertainment content, taking their movie night, sports watching and gaming time to new levels. The new Gradient Light Bars and Gradient Floor Light are designed to be the perfect addition to your TV sync experience. After being configured in the WiZ app, they will match colours to the TV screen corresponding to their physical location and create a fascinating surround lighting experience.

Bring your screen to life
 

The WiZ HDMI sync box with TV backlight is all that the users need for bringing their screens to life. By simply connecting the Sync box to a HDMI media device such as streaming stick, set-top box, and gaming console, and attaching the LED strip to the back of their TV, users can make lights sync with the colours and brightness of the TV screen. No need to put a camera on top of your TV screen and there is no need for a complicated calibration procedure. It supports HDMI 2.0 and video formats up to 4K at 60Hz with HDR10+/Dolby Vision. The Sync box reads the video signal directly from the HDMI input, instantly analyzes the entire screen, and generates ultra-accurate colours on the lights. Featuring a 3-side segmented RGBIC light strip for easy mounting on the back of TV, the HDMI sync box offers two different sizes, fitting TV’s from 55” to 65”, and from 75” to 85”.


The clean setup and personalised experience make the WiZ Sync Box perfect for every style and TV watching occasion. With the 4 preset sync modes - Cinematic, Vibrant, Relaxation, Rhythmic and customizable brightness, colour saturation and intensity, users can set lights to closely follow all the colours with drastic brightness change or to gradually transition while matching colours to the dominant hue on the screen. The HDMI Sync Box works with any WiZ colour-capable light that supports both Wi-Fi and Bluetooth. Users can link as many lights to the Sync Box as they like (they need to be connected to the same Wi-Fi network) and make them sync with TV simultaneously. The Sync Box also has a built-in microphone that can capture audio playing from any source and make lights change colours and brightness with the music. Control is simple via the WiZ app, voice (with Google or Alexa) or the WiZ remote control. Users can also set the auto-switching feature in the app so their TV sync lights will turn on and start syncing automatically whenever the HDMI media source provides a signal.

 

At WiZ, we believe that enhancing your entertainment experience should be as fun and effortless as possible. Our new TV sync and vibrant smart lighting solutions allow users to transform any room into their personalised cinematic paradise. With intuitive controls and seamless integration, we empower everyone to enjoy the magic of smart lighting, making every viewing experience unforgettable."

 

Maikel Klomp

Business Leader of WiZ Connected

Compact design, remarkable ambiance: the Gradient Light Bars 

 

The Gradient Light Bars create captivating lighting in any space. Each light bar can be controlled individually and features a multicolour segment design that displays multiple colours simultaneously, creating beautiful wall-washing effects. Versatile in installation, the Gradient Light Bars come with various mounting brackets, allowing placement horizontally or vertically on counters or desks, or fixed behind TVs and monitors.

Bring colours to any corner: the Gradient Floor Light
  

The Gradient Floor light offers a multicolour segment design and wide beam angle, illuminating any room with stunning wall-washing effects. Its slim, minimalistic design fits effortlessly into any corner, complementing various interiors. Featuring a one-piece design for seamless plug-and-play functionality—no assembly required—.
 

Both the Gradient Light Bars and the Gradient Floor light deliver an engaging atmosphere by syncing colours with video (Sync box required) and with music. With 16 million colours and ready-to-use preset modes like Party, Fireplace, and Ocean, users can set the perfect mood for any occasion. They are Matter compatible so they can also be controlled with Alexa, Google Home and Apple HomeKit.


For more information, please visit: www.wizconnected.com

Availability

 

Products available from July 2025.
 

HDMI sync box with TV backlight for 55”~65” TV

  • Australia: AUD $ 189.95
  • New Zealand: NZD $ 199.99

HDMI sync box with TV backlight for 75”~ 85” TV

  • Australia: AUD $ 239.95
  • New Zealand: NZD $ 249.99

 Gradient Light Bars

  • Australia: AUD $ 119.95
  • New Zealand: NZD $ 139.99

Gradient Floor light

  • Australia: AUD $ 179.95
  • New Zealand: NZD $ 199.99

About Signify

 

Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

Meydan Bridge

More press releases

  • Potential Safety Risks with Highbays

    June 25, 2026

    Potential Safety Risks with Highbays

  • Capital Markets Day 2026

    June 23, 2026

    Capital Markets Day 2026

  • Signify’s first quarter results 2026

    April 24, 2026

    Signify’s first quarter results 2026