Illuminating excellence at the London Aquatics Centre

September 09, 2026

London Aquatics Centre upgrades to next-generation LED lighting with Signify to boost fan experience and enhance energy efficiency

 

  • Future-proof LED solution enhances performance and sustainability 
  • When used at 100% capacity, the upgrade offers upto 60% energy savings
  • Lighting system meets stringent World Aquatics broadcast standards
  • Innovative AR aiming system enables precise installation in a complex architectural setting

 

Guildford, United Kingdom – Signify (Euronext: LIGHT), the world leader in lighting, has delivered a landmark LED lighting upgrade at the London Aquatics Centre to drive performance, energy saving, efficiency, and long-term sustainability at one of the UK’s most iconic sporting venues, also known to be the most technologically advanced and stunning swimming facility in the world.

 

Designed by Zaha Hadid, the London Aquatics Centre was built in 2012 and immediately took its place on the world stage as a venue for that summer’s elite swimming and diving events. More than a decade later, operator Everyone Active undertook a major modernisation project to replace the venue’s legacy lighting system with energy-efficient LED technology. A key requirement was achieving the stringent World Aquatics (formerly FINA) television broadcast standard of 1,500 lux Ev.

To achieve this, Signify partnered with DC Electrical Supply to deploy a lighting system designed for the unique demands of the venue’s architecture. With luminaires suspended up to 40 metres above water, access, precise aiming and adjustment using conventional methods were challenging and time-consuming. While traditional flood lighting approaches could provide general illumination, they lacked the precision and data validation needed to meet the project’s demanding performance requirements.

 

Instead, Signify deployed a proprietary solution designed to translate an on-paper lighting design into real-world accuracy. By combining its advanced ArenaVision LED gen3.5 luminaires with an innovative Augmented Reality (AR) aiming system, Signify enabled installers to accurately align each luminaire, even at heights of up to 40 metres above the pool.

 

A detailed grid over the pool area enabled installers to align each luminaire precisely with the original lighting design. Instead of relying on a visual aiming scope, the installers used a smartphone attached to the luminaire to aim the lights directly at the grid. This approach reduced time spent working at height, improved installation accuracy, and ensured the final lighting performance matched the design intent. Any subsequent adjustments could be made quickly and precisely, delivering measurable and repeatable results.

 

The installation includes 168 ArenaVision luminaires providing the main competition lighting, complemented by 16 UniFlood Flat luminaires that add additional flexibility. The luminaires are paired with a DMX control system to enable immersive and adaptable lighting scenes that enhance sporting events and audience experiences while meeting the requirements of elite competition.

 

The new lighting provides excellent visibility for athletes and fully complies with the World Aquatics broadcast standards, helping the venue maintain its status as a top destination for televised sporting events. Compared with the previous HID lighting system, the LED solution delivers significant energy savings of more than 60% when used in full capacity. The addition of DMX controls also gives venue operators greater flexibility to create engaging experiences for spectators and support a wider range of events.

Having the new LED lighting at the London Aquatics Centre for elite sport is an absolute game changer. Everyone Active has invested £685,000 in the lighting upgrade, working in partnership with global lighting specialist Signify and electrical contractor DC Electrical Supply. With individual control of each light, we can black out the pool, introduce coloured lighting, and follow athletes during events. This gives the venue flexibility to host many more events while future-proofing the facility and maintaining its reputation as a world-class aquatics venue.“

Mark Basker

Regional Contract Manager at Everyone Active

We’re proud to be working alongside Everyone Active and Signify to deliver a lighting solution that supports all ambitions like energy efficiency and sustainability for the iconic venue while ensuring the best fan experience. Given the complexity of access and adjustment within the venue, the solution installed allows for ensuring results to be measurable and repeatable. The key point of difference is how they translate on-paper lighting design into real-world accuracy.“

Darren Clark,

Director at DC Electrical Supply Ltd

The London Aquatics Centre first took its place on the world stage under Signify lighting in 2012. More than a decade later, we are proud to have been chosen once again to help future-proof this iconic venue with a new generation of lighting performance, flexibility, and energy efficiency that will support athletes, spectators, and broadcasters for years to come.“

Simon Wilkinson,

Commercial Leader, Public UK, Signify

The new energy efficient lighting upgrade is a welcome addition to London Aquatics Centre as we embark on the next phase of Queen Elizabeth Olympic Park, focussing on shaping sustainable communities while supporting the Mayor’s ambitions for a greener, cleaner and healthier capital. London Aquatics Centre is a much-loved venue, and Everyone Active’s investment builds on its legacy as an exemplar for televised sport where major swimming events are hosted regularly. It also benefits those who use the space, from local members of the community to world class athletes.“

Mark Camley,

Executive Director for Estate & Neighbourhoods at LLDC

Read all about Sports Lighting here Sports Lighting | Signify United Kingdom

About Signify

 

Signify (Euronext: LIGHT) i

Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers. We proudly bring to market the world’s best lighting brands, from Signify, Philips, Philips Hue, Signify Interact, Signify Dynalite, Color Kinetics and many more. Our advanced products connected systems and services unlock the extraordinary potential of light for brighter lives and a better world. In 2025, we had sales of EUR 5.8 billion, approximately 27,000 employees, and a presence in over 70 markets. We are in the Dow Jones Best-in-Class World Index , earned a CDP ‘A’ score for climate performance and transparency and hold the EcoVadis Platinum rating.

 

News and updates from Signify can be found in the Newsroom, on LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

Meydan Bridge

More press releases

  • Oxford analysis links circular approaches to business benefits in 74% of real-world lighting projects studied

    October 26, 2026

    Oxford analysis links circular approaches to business benefits in 74% of real-world lighting projects studied

  • Signify's third quarter results 2026

    October 23, 2026

    Signify's third quarter results 2026

  • Signify awarded EcoVadis Platinum medal with its highest-ever score of 88

    October 07, 2026

    Signify awarded EcoVadis Platinum medal with its highest-ever score of 88