The significance of intelligent buildings has become especially clear in the post-pandemic era. As companies adjust to new workplace realities, connected systems and the IoT applications built on them become indispensable.
Central to the rise of intelligent buildings is the digitalisation of the physical environment. Digital technologies allow buildings to operate as platforms that deliver various services, from predictive maintenance to real-time energy analytics. These "value services" are made possible by integrating connected systems and cloud-based data processing. By embedding sensors into lighting, HVAC, and security systems, buildings can gather continuous data about usage, occupancy, environmental conditions, and system performance. That data is then processed in the cloud, where it is analysed and visualised to inform better decisions. The result is an environment that evolves in real-time, optimising itself to serve the needs of both people and the organisation.
A smart first step is to swap out the old inefficient legacy warehouse lighting, where it still exists, for new efficient LED lighting. LED lighting can be up to 80% more efficient than traditional lighting, and as LED lighting can last up to 25 times longer than conventional sources, so you also get the benefit of reduced maintenance costs, which due to the ceiling heights in warehouses can be a very costly exercise.
But the possibilities get even brighter, so to speak. When organisations make the switch to LED lighting, a layer of lighting controls can also be added to enable further savings. The lighting levels can be automatically adjusted depending on the activities taking place. These additional energy savings can come from daylight-sensing, scene/task setting and presence/occupancy detection, all of which will help to further reduce the energy consumption of the lighting.
Among all building systems, connected lighting presents a unique opportunity to act as a foundation for intelligent capabilities. Lighting is already present in every building area and can be upgraded with little disruption. When equipped with connected LED technology, lighting becomes far more than a utility—it becomes a strategic part of the infrastructure.
Connected lighting can play a significant role in enabling a building to become even more energy efficient, operationally efficient and sustainable.
One such system is our Interact “connected lighting” system. Intelligent drivers and sensors are embedded into the light fixtures to create either a wired or wireless infrastructure allowing for full remote control and management of the lighting.
A remote cloud-based system can also be used to allow for multiple sites to be connected to one common platform/dashboard. It then becomes much easier to take complete control of all the lighting across multisite and countries, from anywhere, at any time.
The Interact system offers an intuitive dashboard that gives insight into lighting usage and allows users to optimise lighting operations remotely. Interact offers a flexible, cost-efficient, scalable system that meets unique needs and is easy to understand and operate. It is easy to take advantage of IoT technology to suit the needs of every facility. But this is just the beginning.

Intelligent Occupancy sensors which are embedded into the lighting, continuously gather data about presence and footfall within the space. Heat maps can then be simply created to show which areas are being more frequently used and those that are not. This data can not only help the client to further optimise the lighting regimes /levels, but it can also be used to help improve operational costs by optimising stock locations and pick times.
The possibilities do not end here. Environmental sensing is also possible with our smart sensors. Temperature can be continually monitored and optimised, ensuring the right amount of heating and cooling is applied to the space. Similarly, CO2 levels can be monitored to keep an eye on ventilation and air flows.
Platforms like Interact by Signify demonstrate the power of connected lighting as a digital backbone. Interact enables centralised control and monitoring of lighting systems across entire facilities. Through its software, lighting scenes can be adjusted, energy use tracked, and operations optimised for efficiency and comfort.
The full potential of intelligent buildings is unlocked when these systems are integrated into a larger IoT-enabled ecosystem. With the continuous data streams that are collected and stored in a centralised data lake through cloud-connected sensors, facility managers gain real-time insights into how space is used and where the lighting is used the most (or least) enabling them to make evidence-based decisions about layout, staffing, and maintenance. Automated systems can adjust lighting, or temperature based on real-time conditions without human intervention.
In industrial settings, the use of connected lighting in a smart building can transform traditional manufacturing into smart factories. These environments use connected infrastructure to boost productivity, reduce energy consumption, and improve safety. Intelligent lighting systems, for example, can provide high-intensity illumination in areas where precision work is being done and automatically dim in unoccupied spaces to conserve energy.
In the workspace, connected lighting can encourage the shift to smart offices. As more organisations embrace hybrid and flexible work arrangements, office environments must adapt. Intelligent systems allow for dynamic space management, where desks, meeting rooms, and other facilities can be reserved or allocated based on occupancy and demand. Environmental controls such as lighting can be tailored to individual preferences, enhancing comfort and productivity, for example.
Ultimately, the rise of intelligent buildings reflects a broader shift in how we view space. Buildings are no longer seen as fixed structures—they are evolving, data-driven systems that serve a strategic role in business and society. By investing in connected lighting and the platforms that manage them, companies are creating flexible, efficient, and sustainable environments. These buildings do more than house people and operations—they actively support them, adapt to them, and help them thrive.
As we look to the future, it's clear that the most successful environments will not be the largest or the newest but the smartest. Intelligent buildings set the standard for how we live, work, and grow in a world that demands more from our spaces. They are not just changing buildings but redefining what buildings can be.
Signify Global Media relations - Professional Lighting
Claire Phillips
Tel: +44 7956 489081
Email: claire.phillips@signify.com
Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers and lighting for the Internet of Things. Our Philips products, Interact connected lighting systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2022, we had sales of EUR 7.5 billion, approximately 35,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We achieved carbon neutrality in our operations in 2020, have been in the Dow Jones Sustainability World Index since our IPO for six consecutive years and were named Industry Leader in 2017, 2018 and 2019. News from Signify is located at the Newsroom, Twitter, LinkedIn and Instagram. Information for investors can be found on the Investor Relations page.