United Kingdom - English

Why DC-powered lighting matters for modern datacenters

Digital infrastructure has become the backbone of the economy and of daily life itself. Critical processes ranging from streaming media to running financial transactions are powered by an ever-growing web of data centers. These facilities not only support global connectivity but also generate significant employment and tax revenue through their construction, operation, and maintenance.

 

Yet data centers are now facing a triple challenge: rapidly expanding capacity driven by AI workloads, the rising cost of energy, and growing sustainability expectations. To address these pressures, the industry is rethinking its electrical foundations. Direct current (DC) architectures—long the domain of specialized systems—are now emerging as a key enabler of efficiency and resilience.

 

Lighting, often seen as a secondary system, can play a strategic role in this transition. Highly energy-efficient DC-powered LED lighting solutions offer a practical entry point to broader DC adoption, improving overall facility efficiency while advancing sustainability goals.

 

This article explores how lighting can act as both an energy-saving technology and an intelligent infrastructure layer within next-generation data centers.

Evolving data center architectures

A data center must coordinate a complex interplay of servers, networking, power, cooling, and security systems. Traditionally, these systems have relied on alternating current (AC) for power distribution. But as facilities scale to meet rising processing demands, electrical efficiency and power density are becoming critical design priorities.

 

Early data centers used 48 V DC for backup systems—safe, but limited in capacity. Over time, this evolved to 230/277 V AC mains, and later to 380 V DC for internal power distribution. Today, to meet the massive power demands of AI servers, designs are shifting again—to 650 V DC and even 800 V DC architectures.

 

The Open Direct Current Alliance (ODCA) identifies 650 V DC as the optimal voltage for full-building distribution, offering an effective balance between safety and efficiency. Major technology players such as NVIDIA and the Open Compute Project (OCP) are exploring 800 V DC at the rack level, though such implementations still lack the system-wide efficiencies that 650 V DC can deliver when deployed across an entire facility.

 

Beyond data centers, industrial facilities are also adopting 650 V DC systems to cut energy use and improve resilience. This voltage level enables the capture and reuse of braking energy from motor drives and robotics—energy that would otherwise be wasted as heat. Lighting, a constant baseload in production environments, can effectively absorb and use this recovered power, reducing grid demand and operational costs.

 

By integrating lighting, motors, and renewable sources on a shared DC grid, sites achieve a more efficient energy flow while minimizing AC/DC conversion losses. Compared with 400 V AC networks, DC systems use fewer conductors, reduce copper consumption, and lower transmission losses. When combined with solar PV and battery storage, they also boost self-consumption, ensure backup capability, and support flexible energy management.

Why DC power is gaining ground

The case for DC in data centers is both technical and economic:

 

  • Reduced conversion losses
    Traditional AC systems require multiple conversion stages (AC→DC→AC→DC), leading to energy losses of up to 18%
  • Native compatibility
    IT loads such as servers and GPUs inherently operate on DC power
  • Seamless renewable integration
    Solar PV arrays and battery storage produce DC natively, simplifying connection and improving overall system efficiency
  • Simplified infrastructure
    DC eliminates many transformers and rectifiers, cutting installation complexity and improving reliability
  • AI readiness

With surging AI workloads data centers switch to DC power systems.

DC is not merely a power format—it’s a pathway toward more intelligent, efficient, and resilient infrastructure.

Lighting as a gateway to DC infrastructure

Lighting is often the first system that can transition to DC in a data center. Connected LED lighting presents a low-risk, high-impact opportunity to test and scale DC distribution before extending it to mission-critical IT loads.

Key advantages of deploying DC lighting in data centers include:

 

  • Lower CAPEX
    Power cables for DC lighting save 40% on copper. They include only three conductors (L+, L-, PE) but transmit the same power as 400 V, 3-phase AC power cables with five conductors (L1, L2, L3, N, PE), as used in traditional data centers.
  • Lower OPEX
    Power cables for DC lighting avoid 33% of the losses in power cables. since the power is transmitted with only two conductors (L+ and L-) instead of the three conductors of a three-phase AC system at the same current.
  • Resilience and redundancy
    DC lighting can run directly from on-site solar arrays or battery storage, enhancing microgrid resilience during grid disturbances

 

Luminaires and components for DC-powered data centers are available in the marketplace today. For example, Signify has developed a 100 W Xitanium LED driver designed for 620–750 V DC operation and integrated it into a new generation of Pacific LED Gen5 and Maxos Fusion luminaire families. These luminaires deliver up to 165 lm/W efficacy and can be combined with lighting control systems like Signify Interact and Philips Dynalite.. The system’s efficiency can exceed 95% at driver level, with future potential to reach 200 lm/W using ultra-high-efficiency LED modules.

Sustainability and ESG impacts

DC-powered lighting delivers measurable sustainability benefits, including:

 

  • Carbon reduction
    Reduced carbon footprint due to fewer conversion losses and lower material use
  • Eligibility for green certifications
    DC-based systems can contribute to LEED Zero and BREEAM credits
  • Smart optimization
    Connected LED lighting can reduce total lighting energy use by up to 75% through sensors and controls

 

In sustainability reporting and ESG audits, these benefits help hyperscalers (like Amazon Web Services and Microsoft Azure) and colocation providers demonstrate tangible progress toward carbon neutrality and operational efficiency.

Connected lighting as a distributed sensor network

Connected lighting systems have evolved into a powerful digital infrastructure layer that extends far beyond illumination. When LED luminaires are equipped with embedded sensors for parameters such as occupancy, daylight, temperature, humidity, and air quality, they become a dense, facility-wide network for continuous data collection. This distributed sensing capability transforms the lighting grid into a valuable source of real-time insight—covering everywhere in a building where light is needed, without the need for additional sensor deployments.

 

Through open communication protocols such as DALI, BACnet, and MQTT, DC-powered lighting networks integrate seamlessly with building management and data center infrastructure management (DCIM) systems. This interoperability enables unified control and monitoring across the entire facility, supporting applications that drive efficiency and reliability. Predictive maintenance becomes possible through continuous tracking of both environmental conditions and component health, allowing issues to be addressed before they cause downtime. Operational intelligence is enhanced by analyzing occupancy and thermal patterns, optimizing cooling and space utilization in dynamic environments like data halls or industrial production floors.

 

In addition, connected lighting plays an important role in supporting the well-being and performance of personnel. Human-centric or circadian lighting schemes can be tuned to maintain alertness and reduce fatigue during night shifts or extended operations—an important consideration in mission-critical facilities that run 24/7. By combining digital sensing, intelligent control, and human-centered design, connected lighting networks contribute directly to uptime, safety, and productivity—delivering value well beyond the traditional boundaries of illumination.

Deployment models for lighting in data centers

Lighting can be deployed in several configurations, depending on the scale, architecture, and energy strategy of the facility. At the most localized level, data centers with rack-level DC power lighting may be still supplied from an AC mains backbone.

 

At a broader scale, facility-level DC grids integrate lighting into a shared energy ecosystem that may also include solar generation, battery storage, and DC-powered IT infrastructure. In such systems, lighting not only benefits from renewable sources but also contributes to overall grid stability by acting as a controllable base load.

 

In addition, centralized emergency lighting integrated into the DC backbone ensures illumination continuity during power disruptions, reinforcing safety in mission-critical environments.

Business case and ROI

From a financial perspective, DC lighting offers a compelling return on investment:

 

  • Lower installation costs
    through power cables with 40% less copper, simplified wiring and fewer conversion components
  • Reduced OPEX
    driven by reduced energy consumption and maintenance costs
  • Long-term value

from improved resilience, lower PUE, and compliance with ESG mandates

DC lighting as a strategic entry point for data centers

Lighting is no longer just an operational afterthought—it’s a strategic entry point for data centers navigating the next decade of digital growth.

 

DC-powered lighting not only boosts energy efficiency but also supports industrial sustainability goals. It simplifies cabling, aligns seamlessly with renewable DC sources, and transforms lighting from a passive load into an active participant in energy recovery and smart microgrid management. As data centers transition to DC infrastructure, lighting stands out as a practical and high-impact entry point for realizing the full promise of energy-efficient production.

About the author:

Clark Morrow

Ton van de Wiel

 

Global Segment Manager, Intelligent Buildings, Signify

For further information, please contact:

Signify Global Media relations - Professional Lighting
Claire Phillips

Tel: +44 7956 489081

Email: claire.phillips@signify.com

For commercial enquiries:

About Signify

 

Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers and lighting for the Internet of Things. Our Philips products, Interact connected lighting systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2022, we had sales of EUR 7.5 billion, approximately 35,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We achieved carbon neutrality in our operations in 2020, have been in the Dow Jones Sustainability World Index since our IPO for six consecutive years and were named Industry Leader in 2017, 2018 and 2019. News from Signify is located at the Newsroom, Twitter, LinkedIn and Instagram. Information for investors can be found on the Investor Relations page.

Meydan Bridge