Philips equips Chelsea Football Club to become the world’s first top club to use LED floodlights

August 7, 2014

London, UK – Royal Philips (NYSE:PHG, AEX:PHIA), the global leader in lighting, has provided state-of- the-art LED pitch lighting for Chelsea Football Club. Stamford Bridge is the first stadium for a top flight football club equipped with this pioneering lighting system, which will ensure that the stadium continues to be one of the most famous sporting arenas in the world.
 
The Philips ArenaVision LED floodlighting system is an innovative LED pitch lighting solution. It is designed to provide footballers, fans and TV broadcasters with the best possible experience and supports the latest Premier League requirements for TV broadcasting. These include lighting standards for high definition super slow-motion replays, avoiding the flicker synonymous with conventional lamps. Also, unlike the previous metal halide system, the new LED solution can be instantly switched on and off without the need for a warm up period.
 
Ron Gourlay, Chief Executive of Chelsea FC said, “I am delighted to be able to work with Philips on delivering the best possible environment for our supporters to enjoy Chelsea matches in. Once again, Chelsea Football Club is at the forefront of innovation and we look forward to many more memorable games at Stamford Bridge under this new floodlighting system.”
 
Eric Rondolat, CEO of Philips Lighting comments, “The world’s first ever floodlit football match took place in England, so as sports lighting goes digital it is only right that the lighting standard is again being set there. We are witnessing another technology milestone in the modern football game.
 
‘’Our LED pitch lighting meets the new stringent broadcast criteria of the English Premier League in helping to deliver high definition, flicker-free super-slow motion images and ensures that Chelsea delivers the best possible viewing experience to the 40,000 plus fans in the stadium as well as those at home.”
 
The solution includes a dedicated user interface and a control system allowing quick, easy and reliable monitoring of the system and switching between optimal lighting configurations thereby providing complete flexibility and the ability to switch and dim each floodlight individually. The Philips ArenaVision LED control system can also be used to create special entertainment lighting effects that would normally require dedicated stage-lighting, providing the opportunity for the floodlights to be integrated into pre- and post-match light shows to help build the atmosphere and excitement in the stadium.
 
The new LED floodlights deliver flawless lighting, achieving exceptional vertical illuminance on the players and good uniformity of light. In addition to supporting better-quality broadcast images, the club will also benefit from maintenance savings due to the exceptional long life of the LED solution. Typically, metal halide floodlighting lamps should be replaced every three-seasons to maintain the lighting levels required. The Philips LED system is expected to last in excess of 10 seasons.
 
The new lighting was installed during this summer’s break in time for the start of the new football season. Its first match-day use will be on Tuesday, August 12 when Chelsea plays a friendly against Real Sociedad. In addition, the club is also upgrading its lighting at its training ground, installing the same family of Philips LED floodlighting to deliver a similar lighting performance when training as on match days. With the new system it is possible to light specific areas of the training ground to different illuminance levels to create the ideal practice environment for players.
 
Notes to Editors:
  • Philips has been lighting major sporting events for more than 60 years
  • Philips is the world leader in LED and sports lighting, and is responsible for the pitch lighting of over 65% of stadiums involved in major international sports events
  • Philips lit six out of eight venues used in the 2012 EURO tournament
  • 70% of Barclays English Premier League Clubs are floodlit by Philips
  • Philips provided lighting for nine of the 12 stadiums for this summer’s tournament in Brazil
  • 55% of the world’s main football stadiums contain Philips lighting


The world’s first soccer match played under floodlights was on October 14, 1878, at Bramall Lane, Sheffield, between two teams drawn from players from the Sheffield Football Association.
Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

Chelsea FC Daylight

For further information, please contact:

Siarah Khan 
Philips Lighting External Communications
Tel: +44 7792 225948
E-mail: siarah.khan@signify.com 
.

About Royal Philips:

Royal Philips (NYSE: PHG, AEX: PHIA) is a diversified health and well-being company, focused on improving people’s lives through meaningful innovation in the areas of Healthcare, Consumer Lifestyle and Lighting. Headquartered in the Netherlands, Philips posted 2013 sales of EUR 23.3 billion and employs approximately 113,000 employees with sales and services in more than 100 countries. The company is a leader in cardiac care, acute care and home healthcare, energy efficient lighting solutions and new lighting applications, as well as male shaving and grooming and oral healthcare. News from Philips is located at www.philips.com/newscenter.  .

We'd love to hear from you