Signify has 119,445 thousand ordinary shares outstanding and a free float of 97% (as per June 30, 2026).

 

The Dutch Financial Markets Supervision Act requires persons holding a capital and/or voting interest of 3% or more in Signify to disclose such to the Dutch Authority for the Financial Markets (AFM). The AFM processes these disclosures in its publicly available register, which can be found at www.afm.nl. An overview of the relevant holdings for Signify can be found here.