Signify is committed to the following medium-term guidance for the period 2021-2023:

• Yearly comparable sales growth of 0% to 5%

• Adj. EBITA margin of 11% to 13% in 2023

• Free cash flow above 8% of sales for the period 2021-2023

• ROCE of at least 11% for the period 2021-2023