- Smart city programs inhibited by budget limitations, lack of infrastructure and short-term mindsets
- Visionary leadership would have the biggest impact on smart city implementation
- The rewards are high, with examples including the creation of an estimated 47,000 jobs and millions of euros of smart parking revenue in Barcelona
Eindhoven, the Netherlands – Philips Lighting (Euronext: LIGHT), the world leader in lighting, has today published a new report together with SmartCitiesWorld that highlights the drivers and hurdles faced by local authorities considering implementing a smart city program.
The report1 draws on in-depth research with 150 key influencers on city planning from around the world. Naming Singapore, London and Barcelona as the world’s best smart cities, it reveals that visionary leadership is the factor that would make the biggest difference to the success of smart city programs, cited by 56% of respondents. The report highlighted the impact of enlightened leaders inspired by long-term visions, which are inclusive and encourage collaboration between agencies and across departments.
The potential rewards are high, according to the study, which cites Barcelona as a prime example, having created an estimated 47,000 jobs through the implementation of Internet of Things (IoT) systems, saved EUR 42.5 million on water and generated an extra EUR 36.5 million a year through smart parking2.
One in 10 city authorities lack capacity to develop smart city
However, while one in 10 local authority representatives stated that they did not have the capacity to look at developing a smart city program, they are also being held back by budget limitations, a lack of infrastructure, short term planning and a lack of leadership on implementation.
The most common inhibiting factors are budget limitations (23%) and the need for more supporting infrastructure (19%), demonstrating that securing investment in smart city projects is no easy task. But the report suggests that projects that deliver short-term gains as well as providing infrastructure for the long-term can overcome these issues, such as telco-integrated street lighting in San Jose and smart LED streetlights in Los Angeles, which deliver annual cost savings of USD 9 million and will repay the upfront cost within seven years.
Indeed, the report reveals that it is not uncommon for a city to spend 50% of its energy budget on street lighting. Implementing smart lighting technology not only reduces energy consumption, it has also been seen to lower crime rates, support local businesses as well as create a more aesthetically pleasing environment for city dwellers. This is in addition to the cost and environmental benefits.
Cities consume 70% of world’s energy
Realizing the benefits of smart cities is essential. Cities consume 70% of the world’s energy and by 2050 urban areas are set to be home to 6.5 billion people worldwide, 2.5 billion more than today. For cities to remain fit for purpose as the demand on occupancy and energy increases, local authorities must tackle difficult areas including technology, communications, data security and energy usage.
“City authorities face complex and challenging choices concerning infrastructure, balancing the need to maintain existing services while investing in improvements, managing population growth and enhancing sustainability – all within tight budget constraints,” said Jacques Letzelter, Segment Manager at Philips Lighting.
“New technologies can already transform the way cities deliver, operate and maintain public amenities, from lighting and transportation to connectivity and health services. Often, however, adoption is slowed by the division of work and the selection of technology that doesn’t easily work together or integrate with other city services. Fortunately, there are many successful examples of smart city projects that prove these obstacles can be overcome, with the right collaborative approach and integration technologies. These projects show that smart cities can bring about better lives and enhanced safety for their citizens.”
Embracing the IoT
The report also discusses the key role that the burgeoning IoT has to play on smart city success. Revolutionizing the collection of data (35%), revolutionizing communication for accurate service delivery (15%) and managing the strain on urban resources (13%) were ranked as the top three areas where the IoT would be most effective in cities. However, the report notes that the implementation of new technologies and a smart city program is different for each city.
The top three smart cities were all noted for very different strengths in their smart city programs. Singapore was praised for its forward-thinking infrastructure including its buildings, transportation and use of underground space. London was commended for its focus on communities when implementing technology. One respondent described London as “a honey pot of technologies and partnerships.” Barcelona was noted for its top-level government driving change.
“Collaboration is key. For cities to truly benefit from the potential that smart cities offer, a change in mindset is required where local authorities plan longer and across multiple departments,” said Andreas Knobloch, Alliance Specialist at Philips Lighting. “We must think of city-wide systems as one ecosystem working together. At the same time, we all - technologists, local governments, businesses, environmentalists and the general public - must help to build the investment case to enable cities to successfully implement smart city programs.”
The full report is available for download here.
Notes to editors
1 SmartCitiesWorld in association with Philips lighting conducted a survey of over 150 thought leaders between August and September 2017 from over 19 countries worldwide. The survey respondents were CIOs, CTOs, CDOs (as well as new functions addressing: innovation, information, technology, data), Mayors, City Department Heads/Managers, Consultants, Specifiers, architects and consultants. The resulting report “Smart Cities: understanding the challenges and opportunities can be downloaded in full here
2 As reported in https://www.ncbi.nlm.nih.gov/pmc/articles/PMC3987056/