As we look forward to travel picking up again, guests will want to be reassured that their hotel is doing everything it can to neutralize viruses and bacteria. In addition to following physical distancing and mask wearing guidelines, hotels should consider adding extra layers of disinfection to their existing processes.
In the hospitality environment, virus transmission can occur via several methods:
Traditional cleaning methods, using highly effective liquids and sprays, may be sufficient to address some areas. However, hoteliers should consider UV-C lighting to help with the large-scale disinfection of their facilities.
UV-C lighting is a proven disinfectant for air, surfaces and objects. The effectiveness of Signify’s UV-C light sources on the inactivation of SARS-COV-2, the virus that causes COVID-19, was even validated in laboratory testing conducted at the National Emerging Infectious Diseases Laboratories at Boston University1. We have now developed new UV-C luminaires and solutions to help the hospitality sector provide service to their customers in an environment that is designed with safety in mind.
As we resume travel and leisure, it will be critical to instil confidence in guests that everything possible is being done to neutralize viruses and bacteria. Signify is dedicated to helping customers meet the challenges of the “new normal” and be better prepared for the future.
1 Recent study performed by Boston University, in collaboration with Signify Research, shows the vulnerabililty of SARS-CoV-2 to UV-C radiation. The study shows a required dose of around 22 ml/cm2 to inactive SARS-CoV-2 to a Log6 level (https://www.researchsquare.com/article/rs-65742/v1).
January 23, 2024
The Evolution of Healthcare Lighting
November 14, 2023
How lighting technology can help reduce risks to migrating birds
September 15, 2023
Unlocking America’s energy efficiency potential