Spaceship lands in Nanjing? No it’s another Philips lit landmark

    March 17, 2015

    It looks like a giant spaceship or a design from the set of Blade Runner.  This bold construction is the International Youth Culture Centre in Nanjing, China. Transforming the city’s skyline with a 16 million color palette and delighting locals and tourists alike, the façade of the 68-storey building, which houses a five-star hotel and offices, costs less than EUR 114 a day to light. This is because the building uses an energy-efficient dynamic color-changing computer controlled LED lighting system from Philips (NYSE: PHG; AEX: PHIA), the global leader in lighting. In this instance, the computer controlled LED lighting system saves an additional 60% in electricity used, compared to normal LED color lighting.

     
    A total of 700,000 nodes of Philips iColor Flex MX LED lights accentuate the building’s fluidity and curves while Philips Vaya Linear LED lights create the striking vertical lines. The 300 meter high structure looks even taller due to Philips Vaya Flood LED lights which project into the night sky. The lighting system enables the building owners to change colors and create spectacular light shows with a click of a mouse button.

    International Youth Culture Centre in Nanjing, China

    International Youth Culture Centre in Nanjing, China

    For more information, please contact:

    Philips Group Communications
    Santa van der Laarse
    E: santa.van.der.laarse@signify.com 
    Tel: +31653400056

    .

    About Royal Philips

    Royal Philips (NYSE: PHG, AEX: PHIA) is a diversified health and well-being company, focused on improving people’s lives through meaningful innovation in the areas of Healthcare, Consumer Lifestyle and Lighting. Headquartered in the Netherlands, Philips posted 2014 sales of EUR 21.4 billion and employs approximately 105,000 employees with sales and services in more than 100 countries. The company is a leader in cardiac care, acute care and home healthcare, energy efficient lighting solutions and new lighting applications, as well as male shaving and grooming and oral healthcare. News from Philips is located at www.philips.com/newscenter.

    .